Where can I get the Demo applications of the Linux BSP for S32V234?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where can I get the Demo applications of the Linux BSP for S32V234?

2,127 次查看
zhangweikanghus
Contributor III

Hi,expert

     I find that the chapter13 of Auto_Linux_BSP_18.0_User_Manual.pdf, it mentions that there are some demo applications for S32v234 Linux BSP as below picture.But I cannot find the Demo application, can you tell me where I can download the demo application source code?

pastedImage_1.png

0 项奖励
回复
2 回复数

1,906 次查看
794972837
Contributor I

hi, I found some demos here.

  

/home/YourAccount/VisionSDK_S32V2_RTM_1_2_0_HF1/s32v234_sdk/demos/apex

0 项奖励
回复

1,906 次查看
mikedoidge
NXP Employee
NXP Employee

Hello zhangweikanghust@163.com‌,

The demos are part of the Vision SDK. If you downloaded the BSP separately from the VSDK, then you will not have the demos, or the libraries, etc. to support them. Here is a link to download the latest version of the VSDK.  https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32V23-VSDK001E  

Hope it helps,

Mike

0 项奖励
回复