Where can I get the Demo applications of the Linux BSP for S32V234?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I get the Demo applications of the Linux BSP for S32V234?

2,020件の閲覧回数
zhangweikanghus
Contributor III

Hi,expert

     I find that the chapter13 of Auto_Linux_BSP_18.0_User_Manual.pdf, it mentions that there are some demo applications for S32v234 Linux BSP as below picture.But I cannot find the Demo application, can you tell me where I can download the demo application source code?

pastedImage_1.png

0 件の賞賛
返信
2 返答(返信)

1,799件の閲覧回数
794972837
Contributor I

hi, I found some demos here.

  

/home/YourAccount/VisionSDK_S32V2_RTM_1_2_0_HF1/s32v234_sdk/demos/apex

0 件の賞賛
返信

1,799件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello zhangweikanghust@163.com‌,

The demos are part of the Vision SDK. If you downloaded the BSP separately from the VSDK, then you will not have the demos, or the libraries, etc. to support them. Here is a link to download the latest version of the VSDK.  https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32V23-VSDK001E  

Hope it helps,

Mike

0 件の賞賛
返信