When installing SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204, several errors occurred as follow

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

When installing SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204, several errors occurred as follow

1,729 次查看
DiZhang
NXP Employee
NXP Employee

DiZhang_0-1660113542528.png

as the picture show:

An error occurred while collecting items to be installed
session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
Unable to read repository at http://www.pemicro.com/eclipse/updates/com.pemicro.debug.gdbjtag.pne.updatesite/5.2.6/plugins/com.pe....
Read timed out

0 项奖励
回复
3 回复数

1,722 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @DiZhang,

Can you retry after deleting S32DS.3.4\eclipse\p2\org.eclipse.equinox.p2.core\cache\ and S32DS.3.4\eclipse\p2\org.eclipse.equinox.p2.repository\cache\?

Best Regards,

Mike

0 项奖励
回复

1,719 次查看
DiZhang
NXP Employee
NXP Employee

Thank you for your reply. I had solved this problem yet.

I think the reason is that the install sequence of update package is not right.

0 项奖励
回复

1,714 次查看
mikedoidge
NXP Employee
NXP Employee

@DiZhang,

It's possible your installation is missing a required update to the P&E drivers. Please go to Help -> Install New Software and then select 'PEMicro - http://www.pemicro.com/eclipse/updates' to check that you have the latest updates and get them installed, next check that you have the S32K3 Development Package, and then try the S32K3 RTD install again.

Best Regards,

Mike

0 项奖励
回复