What the maximum size of DDR RAM can be installed on S32V234EVB?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What the maximum size of DDR RAM can be installed on S32V234EVB?

2,090 次查看
antonvoloshchuk
Contributor I

What the maximum size of DDR RAM can be installed on S32V234EVB: 2/4 Gbytes, maybe more?

标记 (3)
0 项奖励
回复
2 回复数

1,963 次查看
stanish
NXP Employee
NXP Employee

Hi Anton,

As far as I know DDR memory cannot be extended since they are populated directly on S32V234EVB.

There 2 x 2Gbit DDR chips.

Stan

1,963 次查看
antonvoloshchuk
Contributor I

Thanks for answer.

0 项奖励
回复