What's the meaning of this element in config headers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What's the meaning of this element in config headers

1,458 次查看
hnxiaojuzi
Contributor II

1.bmp

this element is describe in ar0231_donfig.h ,which located in VisionSDK_S32V2xx_RTM_1_1_0/s32v234_sdk/demos/isp/isp_ar0231_max9296b_csi_dcu.

I don't know the exact mean of the element each row.

the commentary is before them is "devID/#bytes/data"

标记 (3)
0 项奖励
回复
1 回复

1,309 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

I'm not much familiar with this stuff - but for me it means: 

device ID enumeration, number of bytes in data area, data (up to 4 bytes). But I don't know for what purpose are data used. For me it looks like as camera initialization commands - used in maxim_user.cpp file (c:\NXP\VisionSDK_S32V2xx_RTM_1_1_1\s32v234_sdk\libs\isp\cam_generic\user\src\ ) 

Jiri

0 项奖励
回复