What does "Program finished with error #-1073741819" mean?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What does "Program finished with error #-1073741819" mean?

ソリューションへジャンプ
2,276件の閲覧回数
9610wk
Contributor I

When I use S32 Flash Tool and click "Upload target and algorithm to hardware...", the software shows an error with "Program finished with error #-1073741819". What does this mean and how can I solve this problem?

图片1.png

0 件の賞賛
返信
1 解決策
2,126件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @9610wk , 

 

Please can you check uninstalling the current version of USB/ FTD drivers and installing newer one. 

 

You can find the latest FTDI driver at : https://ftdichip.com/drivers/d2xx-drivers/

 

Please let me know if it works or not. 

 

Thank you. Kind regards. 

 

-Mehul Patel

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,252件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @9610wk 

The following community post discusses this topic, so please take a look at them. 

 

B.R.

VaneB

0 件の賞賛
返信
2,176件の閲覧回数
9610wk
Contributor I

Hi, VaneB

    Thanks for your reply. I read the listed post but the issue still exists.

    I checked the user guide for the evaluation board, installed 'SW32G2_RTD_4.4_2.0.0_HF04_DS_updatesite_D2107' and 'SW32G2_S32DS_3.4.1_D2104'. I also checked the listed conditions in the post and the check results are as follows.

    1.The USB connection between the PC and the target was attempted on one USB port.

    2.The target is set to ‘serial boot mode’ .

    3.The USB cable and other device are good as they can work on my colleague's PC.

    4.There were no other serial connections active on the same COM port at the same time the S32 Flash Tool was in use.

    5.The COM port be entered using UPPERCASE letters.

    6.None of the DIP switches are damaged.

    7.The error was reported after I clicked 'Upload target and algorithm to hardware...'

    Are there any other possible reasons for this issue? Thanks a lot

0 件の賞賛
返信
2,127件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @9610wk , 

 

Please can you check uninstalling the current version of USB/ FTD drivers and installing newer one. 

 

You can find the latest FTDI driver at : https://ftdichip.com/drivers/d2xx-drivers/

 

Please let me know if it works or not. 

 

Thank you. Kind regards. 

 

-Mehul Patel

0 件の賞賛
返信
2,071件の閲覧回数
9610wk
Contributor I

Hi, Mehul Patel

I'm sorry I only saw your reply today.

I solved the problem by uninstalling S32DS v3.4 and installing S32DS v3.5.

Thanks for your reply.

0 件の賞賛
返信
2,040件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @9610wk , 

 

Great that you were able to solve the issue. 

 

Yes, older version of tool might have issue because of old packages/ drivers and solved the With newer Deign Studio. 

 

Thank you for your reply. Happy coding. 

- Mehul 

0 件の賞賛
返信