Unknown referenced nature: com.freescale.processorexpert.core.expertprojectnature.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unknown referenced nature: com.freescale.processorexpert.core.expertprojectnature.

ソリューションへジャンプ
910件の閲覧回数
CY9
Contributor III

S32DS-S32PLATFORM 

S32D v3.5 

uC: S32K144 

Compile: adc_pal_s32k144 example + FreeMASTER SDK

CY9_0-1729840982159.png

 

Unknown referenced nature: com.freescale.processorexpert.core.expertprojectnature.

Any suggestions?

 

Should I remove these lines? 

or ??

0 件の賞賛
返信
1 解決策
883件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

It is recommended to install S32K1 RTD 2.0.x with S32DS Extensions and Updates in S32DS v3.5.  If the online installation fails, please refer to HOWTO: offline install S32K1 RTD 2.0.0 in S32DS v3.5
 
Or install S32K1 SDK RTM 4.0.3 with S32DS Extensions and Updates in S32DS v3.4.
It is not recommended to install S32K1 SDK 4.0.x in S32DS v3.5According to the currently available information, we don’t have any plan to integrate S32SDK S32K1XX 4.0.x into S32DS 3.5 or above version.
 
I imported adc_pal_s32k144 of SDK 4.0.3 in S32DS v3.4 and did not encounter this warning. It seems that this problem has been fixed in the latest SDK version.
 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
884件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

It is recommended to install S32K1 RTD 2.0.x with S32DS Extensions and Updates in S32DS v3.5.  If the online installation fails, please refer to HOWTO: offline install S32K1 RTD 2.0.0 in S32DS v3.5
 
Or install S32K1 SDK RTM 4.0.3 with S32DS Extensions and Updates in S32DS v3.4.
It is not recommended to install S32K1 SDK 4.0.x in S32DS v3.5According to the currently available information, we don’t have any plan to integrate S32SDK S32K1XX 4.0.x into S32DS 3.5 or above version.
 
I imported adc_pal_s32k144 of SDK 4.0.3 in S32DS v3.4 and did not encounter this warning. It seems that this problem has been fixed in the latest SDK version.
 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信