Unable to find SCB in EmbSys Registers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to find SCB in EmbSys Registers

Jump to solution
1,312 Views
Janeting123
Contributor I

I encountered the same problem as this post.

https://community.nxp.com/t5/S32-Design-Studio/these-is-no-SCB-registers-in-peripheral-registers-vie...

Snipaste_2024-05-13_16-50-28.png

The S32DS version I am using is 3.4. The installed extensions are as followsSnipaste_2024-05-13_16-33-58.png

 

0 Kudos
Reply
1 Solution
1,271 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Janeting123 

To view the information in the Peripheral Registry view is necessary to start a debug session. Could you check if you can see the information when debugging any example code?

View solution in original post

0 Kudos
Reply
3 Replies
1,297 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Janeting123 

I tested it with S32DS v3.4 and S32K3XX RTD v2.0.1 and there is no issue. Please instead of using the EmbSys Registers view use the Peripherals Registers view. 

VaneB_1-1715631148899.png

Additionally, the S32K3XX RTD v4.0.0 P20 was developed and tested with S32DS v3.5, so, its functionality is not guaranteed in older IDE versions.

 

B.R.

VaneB

 

0 Kudos
Reply
1,284 Views
Janeting123
Contributor I

This is my peripheral register and it is emptySnipaste_2024-05-14_09-54-25.png

0 Kudos
Reply
1,272 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Janeting123 

To view the information in the Peripheral Registry view is necessary to start a debug session. Could you check if you can see the information when debugging any example code?

0 Kudos
Reply