Unable to configure the peripherals using "ConfigTool" option in the S32 Design Studio IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to configure the peripherals using "ConfigTool" option in the S32 Design Studio IDE

Jump to solution
4,698 Views
Anilpatil_SasvaAuto
Contributor IV

Hello Team,

I am trying to configure the peripherals using the "ConfigTool" provided in the S32 Design Studio IDE. However, I'm encountering errors and am unable to complete the configuration.

Could you please check and let me know why these errors are occurring? I would appreciate it if you could provide a solution. I have attached the relevant files for your reference. Thank you!

0 Kudos
Reply
1 Solution
4,436 Views
Anilpatil_SasvaAuto
Contributor IV
0 Kudos
Reply
13 Replies
4,445 Views
Anilpatil_SasvaAuto
Contributor IV

Please provide the solution

0 Kudos
Reply
4,438 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please show me a screenshot of the error.

Some companies' IT restricts http access, Did you change Available S32DS Software Sites to https

0 Kudos
Reply
4,690 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Seems that you want to import the S32K1 SDK 4.0.3 based project. 

Please install S32DS v3.4 + S32K1 SDK 4.0.3 by refer to the discussion in Where can I find it?S32_SDK_S32K1xx_RTM_4.0.3

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
4,664 Views
Anilpatil_SasvaAuto
Contributor IV
I am not able to find the "S32K1 SDK 4.0.3" and install
0 Kudos
Reply
4,650 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

The S32 SDK for S32K1xx RTM 4.0.3 should be listed in Extensions and Updates

0 Kudos
Reply
4,577 Views
Anilpatil_SasvaAuto
Contributor IV
Unable to install, getting error
0 Kudos
Reply
4,553 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please show me a screenshot of the error.

Some companies' IT restricts http access, Did you change Available S32DS Software Sites to https

0 Kudos
Reply
4,437 Views
Anilpatil_SasvaAuto
Contributor IV

Please find the error details as attached

Screenshot 2025-05-30 160344.png

0 Kudos
Reply
4,431 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please check if the S32K1xx development package has been installed?
If not, please install the S32K1xx development package first. Refer to:
 S32 Design Studio 3.4 S32K1xx Service Pack 1 (SW32K1_S32DS_3.4.1_D2106.zip) 

0 Kudos
Reply
4,424 Views
Anilpatil_SasvaAuto
Contributor IV

I have changed to http but no use still same issue

0 Kudos
Reply
4,411 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Do not change it to http.   Please change it to https!

Did you install S32K1xx development package by refer to https://community.nxp.com/t5/S32K/Trying-to-install-the-S32SDK-S32K1xx-RTM-4-0-2-SDK-extension/td-p/... ?

S32K1xx development package.png

After you have installed SW32K1_S32DS_3.4.1_D2106.zip offline, you should be able to install S32SDK S32K1XX RTM 4.0.3 online via S32DS Extensions and Updates.

0 Kudos
Reply
4,167 Views
Anilpatil_SasvaAuto
Contributor IV
Thanks, installed successfully
0 Kudos
Reply
4,437 Views
Anilpatil_SasvaAuto
Contributor IV

FYI

0 Kudos
Reply