Unable to configure the peripherals using "ConfigTool" option in the S32 Design Studio IDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Unable to configure the peripherals using "ConfigTool" option in the S32 Design Studio IDE

跳至解决方案
3,789 次查看
Anilpatil_SasvaAuto
Contributor III

Hello Team,

I am trying to configure the peripherals using the "ConfigTool" provided in the S32 Design Studio IDE. However, I'm encountering errors and am unable to complete the configuration.

Could you please check and let me know why these errors are occurring? I would appreciate it if you could provide a solution. I have attached the relevant files for your reference. Thank you!

0 项奖励
回复
1 解答
3,527 次查看
Anilpatil_SasvaAuto
Contributor III
0 项奖励
回复
13 回复数
3,536 次查看
Anilpatil_SasvaAuto
Contributor III

Please provide the solution

0 项奖励
回复
3,529 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Please show me a screenshot of the error.

Some companies' IT restricts http access, Did you change Available S32DS Software Sites to https

0 项奖励
回复
3,781 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Seems that you want to import the S32K1 SDK 4.0.3 based project. 

Please install S32DS v3.4 + S32K1 SDK 4.0.3 by refer to the discussion in Where can I find it?S32_SDK_S32K1xx_RTM_4.0.3

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
3,755 次查看
Anilpatil_SasvaAuto
Contributor III
I am not able to find the "S32K1 SDK 4.0.3" and install
0 项奖励
回复
3,741 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

The S32 SDK for S32K1xx RTM 4.0.3 should be listed in Extensions and Updates

0 项奖励
回复
3,668 次查看
Anilpatil_SasvaAuto
Contributor III
Unable to install, getting error
0 项奖励
回复
3,644 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Please show me a screenshot of the error.

Some companies' IT restricts http access, Did you change Available S32DS Software Sites to https

0 项奖励
回复
3,528 次查看
Anilpatil_SasvaAuto
Contributor III

Please find the error details as attached

Screenshot 2025-05-30 160344.png

0 项奖励
回复
3,522 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Please check if the S32K1xx development package has been installed?
If not, please install the S32K1xx development package first. Refer to:
 S32 Design Studio 3.4 S32K1xx Service Pack 1 (SW32K1_S32DS_3.4.1_D2106.zip) 

0 项奖励
回复
3,515 次查看
Anilpatil_SasvaAuto
Contributor III

I have changed to http but no use still same issue

0 项奖励
回复
3,502 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Do not change it to http.   Please change it to https!

Did you install S32K1xx development package by refer to https://community.nxp.com/t5/S32K/Trying-to-install-the-S32SDK-S32K1xx-RTM-4-0-2-SDK-extension/td-p/... ?

S32K1xx development package.png

After you have installed SW32K1_S32DS_3.4.1_D2106.zip offline, you should be able to install S32SDK S32K1XX RTM 4.0.3 online via S32DS Extensions and Updates.

0 项奖励
回复
3,258 次查看
Anilpatil_SasvaAuto
Contributor III
Thanks, installed successfully
0 项奖励
回复
3,528 次查看
Anilpatil_SasvaAuto
Contributor III

FYI

0 项奖励
回复