There is a problem installing S32DS_ARM_v2018.R1_UP9.zip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

There is a problem installing S32DS_ARM_v2018.R1_UP9.zip

1,844 Views
r_kikuchi
Contributor I

According to this page (https://community.nxp.com/docs/DOC-342805)
Problems will occur when installing S32DS_ARM_v2018.R1_UP9.zip.
Please tell me how to respond.

0 Kudos
Reply
4 Replies

1,555 Views
zhiqunhu
Contributor III

I have the same problem.

I have tried with both online and offline methods described in the link: (https://community.nxp.com/docs/DOC-342805).

Also, I have tried to uninstall S32 Design Studio for ARM Version 2018.R1 then reinstalled it then tried both methods for UP9.zip again, but I still have the same problem shown below.

Not sure what else can be tried?

pastedImage_1.png

0 Kudos
Reply

1,555 Views
r_kikuchi
Contributor I
Thank you.
I uninstalled "S32 Design Studio for ARM Version 2018.R1" and installed it again.
Run "Help -> Install New Software -> Add -> Archive -> S32DS_ARM_v2018.R1_UP8.zip".
Run "Help -> Install New Software -> Add -> Archive -> S32DS_ARM_v2018.R1_UP9.zip".
0 Kudos
Reply

1,555 Views
stanish
NXP Employee
NXP Employee

Hi Ryoi,

First please make sure you installed the latest S32DS for arm 2018.R1: 

S32 Design Studio for ARM 2018.R1 (Windows/Linux) released! 

and then use online or offline  method (described in the document) to install Update 9

https://community.nxp.com/docs/DOC-342805 

There has been an issue with online update method reported recently but it should be fixed now.

Please let us know if you observe any issues.

Regards,

Stan

0 Kudos
Reply

1,555 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

is in your S32DS_ARM_v2.0 directory installed S32DS_ARM_v2018.R1? By default latest S32DS version uses as home folder S32DS_ARM_v2018.R1.

Jiri 

0 Kudos
Reply