The program I used is the example project with the name of wdg_pal_interrupt_mpc5744p. When I try to build the project, the type bool can not be resolved. close the project and re-open it ,the error will disappear. when open the file fccu_driver.c ,the bool err will appear again ,I have no idea to solve this issue.....And how to solve it ?