The program I used is the example project with the name of wdg_pal_interrupt_mpc5744p. When I try to build the project, the type bool can not be resolved. close the project and re-open it ,the error will disappear.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The program I used is the example project with the name of wdg_pal_interrupt_mpc5744p. When I try to build the project, the type bool can not be resolved. close the project and re-open it ,the error will disappear.

1,369 Views
996028202
Contributor I

The program I used is the example project with the name of  wdg_pal_interrupt_mpc5744p. When I try to build the project, the type bool can not be resolved. close the project and re-open it ,the error will disappear.  when open the file fccu_driver.c ,the bool err will appear again ,I have no idea to solve this issue.....And how to solve it ?

pastedImage_1.png

0 Kudos
Reply
0 Replies