The S32R294 chip executes abnormally when powered on and off after using Lauterbach to burn code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The S32R294 chip executes abnormally when powered on and off after using Lauterbach to burn code

372件の閲覧回数
Jack_112233
Contributor I

1. Using Lauterbach to burn code into the board, but after powering on and restarting, the code actually runs the program that was previously burned. If do not restart, i can still debug normally.

2. Another problem is that after the Lauterbach cpu is reset, the boot address remains 0x00000000. Do you know if the S32r has a setting like tricore bmhd?

Jack_112233_0-1714275473520.png

 

0 件の賞賛
返信
1 返信

343件の閲覧回数
rweiss
Contributor V

Try this:

SYStem.Option ResBreak OFF
SYStem.Up

Best regards,
Reinhard

0 件の賞賛
返信