SW32XX-IPCF-EAR_0.8.8 installation in S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SW32XX-IPCF-EAR_0.8.8 installation in S32DS

2,239 Views
Somasundaram_Vadivelu
Contributor III

I want to install SW32XX-IPCF-EAR_0.8.8 in S32DS since the latest version of IPCF doesn't support multicore. But the package SW32XX-IPCF-EAR_0.8.8 doesn't have any zip file, so I am not able to install it in the "Install software extension" in S32DS. I followed the release notes in the SW32XX-IPCF-EAR_0.8.8 package (It says to install it under the software folder under the s32ds), but I don't see the ipcf example under the (File -> Open project from example).
Any help will be appreciated.

Thanks

 

 

0 Kudos
Reply
8 Replies

2,220 Views
nxf45396
NXP Employee
NXP Employee

All IPCF versions support multicore elf. The RTD v0.9.0 is supporting only multicore with single elf. In March IPCF will release the new version what will support RTD v1.0.0 and multiple elf.

IPCF EAR 0.8.8 is installing with executable file (no update site) and can be used with S32SDK_S32G_EAR_0.8.0

best regards
Costin

OCV
0 Kudos
Reply

2,216 Views
Somasundaram_Vadivelu
Contributor III

Hi,

Thanks for the reply. 
If I understood you currently, the new version of IPCF will have multiple elf support in March.
Can you be a bit more elaborate on how to install IPCF EAR 0.8.8 in S32DS v3.3? I am new to S32DS , so would really appreciate it.

Thanks

 

0 Kudos
Reply

2,214 Views
Somasundaram_Vadivelu
Contributor III

I looked into the user manual of IPCF EAR 0.8.8, where it says to install under "software" folder of S32DS.
I did that but I can't find the ipcf example...

 

0 Kudos
Reply

2,198 Views
nxf45396
NXP Employee
NXP Employee

IPCF example project  cannot be imported because SDK or IPCF package is not installed correct in DS32.

Please check if S32SDK S32G EAR 0.8.0 is installed :  Windows -> Preferences -> S32 Design Studio -> SDK Management.

sdk_check.PNG

 
 
 

Check also if ipcf example is in S32SDK S32G EAR 0.8.0 example directory.

If S32SDK S32G EAR 0.8.0 is not installed, you must install it and then install again IPCF EAR 0.8.8.

OCV
0 Kudos
Reply

2,186 Views
Somasundaram_Vadivelu
Contributor III

I installed S32SDK S32G EAR 0.8.0 , as seen below:

 

error.png

I installed IPCF EAR 0.8.8 in the location mentioned in the manual:
location.png

But still I can't see the ipcf example in my S32 Design Studio.

 

 

0 Kudos
Reply

2,176 Views
nxf45396
NXP Employee
NXP Employee

That installer is for AutosarOS or sample with make file.

Please search in nxp.com for S32SDK_S32G274A_IPCF_EAR_0.8.8.exe and install it.

Please read also this.

Best regards

 

OCV
0 Kudos
Reply

2,109 Views
mohammedZaki2021
Contributor I

The link says Access denied

Tags (1)
0 Kudos
Reply

2,172 Views
Somasundaram_Vadivelu
Contributor III

Hi,
Thanks for the reply.
I searched for S32SDK_S32G274A_IPCF_EAR_0.8.8.exe in nxp.com and couldn't find it. It will be great if you can post the link here. I don't have access to the link you mentioned in the above post.

0 Kudos
Reply