SDK is not showing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SDK is not showing

跳至解决方案
4,073 次查看
RajCS
Contributor I

Installed S32DS V4,

as per manual installed the necessary SW,

During project creation unable to see the SDK

 

Followed the steps from the below document

RajCS_0-1712053543088.png

 #nxp S32G2 

0 项奖励
回复
1 解答
4,044 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you help us share with us which RTD package have you installed? Are you able to see available examples under your setup? Which GCC version did you choose in the previous window? We can also recommend the following HOWTO on this same regard:

HOWTO: Create a Blinking LED application project for S32G using S32 RTD No AUTOSAR - NXP Community

Please, let us know.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,279 次查看
RajCS
Contributor I

HI @Daniel-Aguirre ,

 

There are 2 issues I'm facing.

I connected Micor USB cable to PC and J4 connector. USB is not detected.

 

RajCS_0-1713793736667.png

2)Build is incomplete

 

RajCS_1-1713793811989.png

 

 

 

 

0 项奖励
回复
3,263 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

It seems that this issues are the same as the community thread shown below:

S32G3 board ,unable to find the FSL image is not available in SD card - NXP Community

Information has been provided under the above community thread.

Please, let us know.

0 项奖励
回复
4,045 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you help us share with us which RTD package have you installed? Are you able to see available examples under your setup? Which GCC version did you choose in the previous window? We can also recommend the following HOWTO on this same regard:

HOWTO: Create a Blinking LED application project for S32G using S32 RTD No AUTOSAR - NXP Community

Please, let us know.

0 项奖励
回复
4,025 次查看
RajCS
Contributor I
Hi @Daniel-Aguirre
I have tried same thing,but no luck. Pls let me know if you need any other details.
0 项奖励
回复
4,018 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback.

Can you help us share with us which RTD package have you installed? Are you able to see available examples under your setup? Which GCC version did you choose in the previous window?

Please, let us know.

0 项奖励
回复