S32k322 ADC Internal Temperature issue in S32Design studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k322 ADC Internal Temperature issue in S32Design studio

Jump to solution
327 Views
praveen_ext
Contributor II

Hi,
I configured the 14‑bit ADC for internal temperature sensing, but the RTD temperature sensing macro is defined only for 12‑bit resolution and uses a 12‑bit temperature instance in Adc_Sar_Ip.h and Adc_Sar_Ip.c. Because of this, the calculated temperature, raw ADC reading, and measured voltage are oscillating and not correct. Should the RTD function automatically switch to 14‑bit when I configure 14‑bit ADC, or do I need to define a 14‑bit resolution macro and update the API function manually? here by attached images for your reference.

Read Value while testingRead Value while testingS32 DS Periphral tabS32 DS Periphral tabRTD FunctionRTD Function

Tags (1)
0 Kudos
Reply
1 Solution
290 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The note[4] of section 10.1 SAR_ADC if S32K3 DataSheet Rev13 list:
TUE spec for precision and standard channels is based on 12-bit level resolution.

There is no TUE spec based on 14-bit level resolution.  Therefore, the RTD temperature sensing macro is defined only for 12‑bit resolution and uses a 12‑bit temperature instance in Adc_Sar_Ip.h and Adc_Sar_Ip.c. You need to modify the RTD API yourself.

Please note TS_TADCSA (Required ADC sampling time Required ADC sampling time specified by parameter TS_TADCSA needs to be used at the ADC conversion to guarantee the specified accuracy. A smaller sampling time leads to a less accurate result.

TS_TADCSA Required ADC sampling time 10.4 Temperature Sensor.png

There are 2 methods to reduce the instability of TempSensor CH conversion data:
1.The ADC conversion clock can be set as Module_Clock(Core_CLK 160MHz)/4=40MHz.
2.The ADC Sample Time can be increased instead of using the default value. (Increase the value of Adc Unit Normal Sampling Duration)

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
291 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The note[4] of section 10.1 SAR_ADC if S32K3 DataSheet Rev13 list:
TUE spec for precision and standard channels is based on 12-bit level resolution.

There is no TUE spec based on 14-bit level resolution.  Therefore, the RTD temperature sensing macro is defined only for 12‑bit resolution and uses a 12‑bit temperature instance in Adc_Sar_Ip.h and Adc_Sar_Ip.c. You need to modify the RTD API yourself.

Please note TS_TADCSA (Required ADC sampling time Required ADC sampling time specified by parameter TS_TADCSA needs to be used at the ADC conversion to guarantee the specified accuracy. A smaller sampling time leads to a less accurate result.

TS_TADCSA Required ADC sampling time 10.4 Temperature Sensor.png

There are 2 methods to reduce the instability of TempSensor CH conversion data:
1.The ADC conversion clock can be set as Module_Clock(Core_CLK 160MHz)/4=40MHz.
2.The ADC Sample Time can be increased instead of using the default value. (Increase the value of Adc Unit Normal Sampling Duration)

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply