S32V234 access to OALSRAM gives Bus error (QNX)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32V234 access to OALSRAM gives Bus error (QNX)

1,351件の閲覧回数
ankitkumar_gand
Contributor I

I am trying use VSDK for S32V234 on QNX. OAL kernel driver looks fine, but while accessing it through OAL library gives bus error.

I am creating these memory regions

  {"/memory/below4G/ram/oalddr0", 0x8B000000, 0x05000000, 0, 0x1000, 0 ,1},

  {"/memory/below4G/ram/oalddr1", 0xCB000000, 0x05000000, 1, 0x1000, 0, 1},

  {"/memory/below4G/oalsramS", 0x3E800000, 0x00300000, 2, 0x8, 1, 0},

  {"/memory/below4G/oalsramM", 0x3EB00000, 0x00100000, 3, 0x8, 1, 0}

Access to OALDDR0/1 is fine, but access to OALSRAMS/M doesn't work.

 

handle_oal = OAL_MemoryAllocFlag(1024, OAL_MEMORY_FLAG_ALIGN(ALIGN2_CACHELINE)|OAL_ALLOC_SRAM_SINGLE);

Thanks

タグ(3)
0 件の賞賛
返信
1 返信

1,178件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi ankitkumar.gandhi@nio.io,

This is not the correct community to post S32V2 questions.

Moreover, we have stopped supporting S32V2 community group. But we still support S32V2 question using our ticketing system.

For future questions, please create the request at www.nxp.com/support using Support Requests option. Our experts will help you.

Thank you for understanding.

Mike

0 件の賞賛
返信