S32V234 VSDK isp_ov10640_quad work with max96705

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32V234 VSDK isp_ov10640_quad work with max96705

1,430 Views
liu_jialu1
Contributor II

S32V234 VSDK demo 'isp_ov10640_quad' work with "max9286+max9271*4", but my camera's serializer is "max96705", ii2c read serializer and OV16040 CHIP_ID failed, detail information in attached file.

debug environment:

          hardware: S32V234EVB + MAX9286S32V234DB + LI-OV10640-490-GMSL-055H

          software: S32V234 VSDK  isp_ov10640_quad demo。

Any clear difference with max9271 & max96705? datasheet said they arm compatible.

Labels (3)
0 Kudos
2 Replies

770 Views
xiafeng_luo
Contributor I

hi,i met the same questions. After one year later ,NXP still not solve this problem...i am so surprised.  

0 Kudos

770 Views
KushalShahNXP
NXP Employee
NXP Employee

Hi,

This is not the correct community to post S32V2 questions. 

Moreover, we have stopped supporting S32V2 community group. But we still support S32V2 question using our ticketing system.

For future questions, please create the request at www.nxp.com/support using Support Requests option. Our experts will help you.

 

Thank you for understanding.

 

Regards,

Kushal

0 Kudos