S32M RTD support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32M RTD support

4,580 Views
hns80
Senior Contributor I

Version 3.0.0 P07 claims to support S32M. I installed it, but cannot select anything other than S32K when I create a new project. There isn't any example code available, either. 

How can I get a version of the RTDs that supports the S32M?

 

0 Kudos
Reply
3 Replies

4,517 Views
hns80
Senior Contributor I

When I try to install these, I receive an error:

Operation details Software being installed: com.nxp.RTD.S32M276.root.feature.feature.group 3.0.0.202303311831 Missing requirement: com.nxp.RTD.S32M276.root.feature.feature.group 3.0.0.202303311831 requires 'org.eclipse.equinox.p2.iu; com.nxp.s32ds.s32m2.dev.feature.feature.group 1.0.0' but it could not be found

 

I have the following installed:

RTD S32M276 3.0.0.202306300010 com.nxp.RTD.S32M276.feature.feature.group NXP Semiconductors, Inc.
S32 Design Studio 3.5.3.202306291736 com.nxp.s32ds.platform.ide.feature.feature.group NXP
S32 Design Studio Tools 3.5.3.202306291736 com.nxp.s32ds.platform.ide.tools.feature.feature.group NXP
S32DS Product 3.5.0.202207261815 com.nxp.s32ds.platform.ide.product NXP

What am I missing?

 

0 Kudos
Reply

4,501 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for the information.

The missing package "com.nxp.s32ds.s32m2.dev.feature.feature.group 1.0.0" is the development package for S32M platforms. It seems that it is not installed on your setup.

If you cannot find it on your available SW, then help us contacting your local NXP FAE/DBM, for them to verify if your account has the available information.

Please, let us know.

0 Kudos
Reply

4,538 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Once you add the "SW32K3_RTD_R21-11_3.0.0_P07_D2306_DS_updatesite.zip" to S32DS v3.5 you should see both S32K3 and S32M2 RTD's. You should install the S32M RTD itself. The RTD version supports the platform, but it is through a different package, as seen below:

DanielAguirre_0-1689272633402.png

Have you installed these S32M specific packages?

Please, let us know.

0 Kudos
Reply