S32K3XX example project not found in S32DS 3.5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K3XX example project not found in S32DS 3.5

跳至解决方案
4,002 次查看
AllenLiao
Contributor I

Hi, 

We want to create a project from example but in the" New>S32DS Project from Example" we can't find any example.

AllenLiao_0-1684289039398.png

And installed extensions as below:

AllenLiao_2-1684289201834.png

 

Best Regards,

Allen

 

0 项奖励
回复
1 解答
3,956 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @AllenLiao , 

 

Please can you check and provide your workspace log information from the path : 

..\S32DS.3.5\_S32 Design Studio for S32 Platform 3.5_installation\Logs. 

 

Also, Please can you provide screenshot or information about what packages you have installed.

Mehul_Patel_NXP_1-1684772014405.png


Also, please can you provide information which S32K3 device you are planning to use? You would require to use relevant package for the your device. 

Thank you. Kind regards.

- Mehul Patel

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,957 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @AllenLiao , 

 

Please can you check and provide your workspace log information from the path : 

..\S32DS.3.5\_S32 Design Studio for S32 Platform 3.5_installation\Logs. 

 

Also, Please can you provide screenshot or information about what packages you have installed.

Mehul_Patel_NXP_1-1684772014405.png


Also, please can you provide information which S32K3 device you are planning to use? You would require to use relevant package for the your device. 

Thank you. Kind regards.

- Mehul Patel

0 项奖励
回复
3,195 次查看
feman5012
Contributor II

the same problems, log and intalled plugins are listed below.

0 项奖励
回复