S32K14x CAN message buffers not sending data at same rate with multiple devices and drops frames

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K14x CAN message buffers not sending data at same rate with multiple devices and drops frames

Jump to solution
1,281 Views
m_karthikeyan
Contributor III

In the S32K CAN example project the CAN init initializes all message buffer to 0x0

But the Data sheet wants to start from INACTIVE command for Transfer buffer, but marking it 0x0 makes it a receive buffer, right?


for(i=0; i<128; i++ )
{ /* CAN0: clear 32 msg bufs x 4 words/msg buf = 128 words */
CAN0->RAMn[i] = 0; /* Clear msg buf word */
}
/**** SHOULD WE DO the BELOW initialization, to start the transfers as IDLE/transmit command*/
/*Mark Message buffers 0-3 as TX transfer message buffer*/
CAN0->RAMn[ 0*MSG_BUF_SIZE + 0] = 0x08000000;
CAN0->RAMn[ 1*MSG_BUF_SIZE + 0] = 0x08000000;
CAN0->RAMn[ 2*MSG_BUF_SIZE + 0] = 0x08000000;
CAN0->RAMn[ 3*MSG_BUF_SIZE + 0] = 0x08000000;

 

We have added a 10ms delay and sent a frame with CAN message buffer 0, but sometimes its not sent when there are multiple devices in the bus, doing exact the same [Sending data every 10ms] the rate is mostly 10ms, some times it goes 20,30,40,100,200.

https://www.nxp.com/docs/en/application-note/AN12842.pdf

Does it with a dequeue buffer extensively.

 

handles CAN message buffers differently

From the Reference manual https://www.nxp.com/webapp/Download?colCode=S32K1XXRM&location=null

 

I got the following

"Check whether the respective interrupt bit is set and clear it.
2. If the MB is active (transmission pending), write the ABORT code (0b1001) to the
CODE field of the Control and Status word to request an abort of the transmission.
3. Wait for the corresponding IFLAG bit to be asserted by polling the CAN_IFLAG
register, or by the interrupt request if enabled by the respective IMASK bit.
4. Read back the CODE field to check if the transmission was aborted or transmitted
(see Transmission abort mechanism).
5. Clear the corresponding interrupt flag.
6. Write the ID register (containing the local priority if enabled via MCR[LPRIO_EN]).
7. Write payload data bytes.
8. Configure the Control and Status word with the desired configuration.
• Set ID type via MB_CS[IDE].
• Set Remote Transmission Request (if needed) via MB_CS[RTR].
• If CAN_MCR[FDEN] is enabled, also configure the MB_CS[EDL] and
MB_CS[BRS] fields. For details about the relationship between the written value
and transmitted value of the MB_CS[ESI] field, see Table 53-25.1
• Activate the message buffer to transmit the CAN frame by setting
MB_CS[CODE] to 0xC.
• Set Data Length Code in bytes via MB_CS[DLC]. See Table 53-12 for detailed
information." 

Should we abort the transfers if its not INACTIVE, tried that too with 2 alternating message buffers 0 & 1 with a delay NOT POLLING IFLAG still we observe the data not sent sometimes could you help with a cleaner example for CAN transfer. 

 

 

/*
 * Copyright (c) 2014 - 2016, Freescale Semiconductor, Inc.
 * Copyright (c) 2016 - 2018, NXP.
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions are met:
 *
 * 1. Redistributions of source code must retain the above copyright notice,
 *    this list of conditions and the following disclaimer.
 *
 * 2. Redistributions in binary form must reproduce the above copyright notice,
 *    this list of conditions and the following disclaimer in the documentation
 *    and/or other materials provided with the distribution.
 *
 * 3. Neither the name of the copyright holder nor the names of its contributors
 *    may be used to endorse or promote products derived from this software
 *    without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY NXP "AS IS" AND ANY EXPRESSED OR
 * IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES
 * OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
 * IN NO EVENT SHALL NXP OR ITS CONTRIBUTORS BE LIABLE FOR ANY DIRECT,
 * INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES
 * (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
 * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
 * HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT,
 * STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING
 * IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
 * THE POSSIBILITY OF SUCH DAMAGE.
 */

#include "device_registers.h"	/* include peripheral declarations */
#include "FlexCAN.h"

uint32_t  RxCODE;              /*< Received message buffer code 			*/
uint32_t  RxID;                /*< Received message ID 					*/
uint32_t  RxLENGTH;            /*< Recieved message number of data bytes 	*/
uint32_t  RxDATA[2];           /*< Received message data (2 words) 		*/
uint32_t  RxTIMESTAMP;         /*< Received message time 					*/

void FLEXCAN0_init(void)
{
#define MSG_BUF_SIZE  4		/* Msg Buffer Size. (CAN 2.0AB: 2 hdr +  2 data= 4 words) */
  uint32_t   i=0;

  PCC->PCCn[PCC_FlexCAN0_INDEX] |= PCC_PCCn_CGC_MASK; /* CGC=1: enable clock to FlexCAN0 */

  CAN0->MCR |= CAN_MCR_MDIS_MASK;         /* MDIS=1: Disable module before selecting clock 	*/
  CAN0->CTRL1 &= ~CAN_CTRL1_CLKSRC_MASK;  /* CLKsrc=0: Clock Source = SOSCDIV2				*/
  CAN0->MCR &= ~CAN_MCR_MDIS_MASK;        /* MDIS=0; Enable module config. (Sets FRZ, HALT)	*/

  while (!((CAN0->MCR & CAN_MCR_FRZACK_MASK) >> CAN_MCR_FRZACK_SHIFT))  {}
	/*!
	 * Good practice:
	 * ===================================================
	 * wait for FRZACK=1 on freeze mode entry/exit
	 */
  CAN0->CTRL1 = 0
      #if defined(S32K11x_SERIES)
      |CAN_CTRL1_PRESDIV(4)   /* PRESDIV=4: Sclock=PEclock/(PRESDIV+1) = 40MHz/5 = 8MHz    */
      #endif
      |CAN_CTRL1_PSEG2(3)	    /* Configure for 500 KHz bit time 								*/
		  |CAN_CTRL1_PSEG1(3) 		/* Time quanta freq = 16 time quanta x 500 KHz bit time= 8MHz 	*/
		  |CAN_CTRL1_PROPSEG(6)		/* PRESDIV+1 = Fclksrc/Ftq = 8 MHz/8 MHz = 1 					*/
		  |CAN_CTRL1_RJW(3)			/*    so PRESDIV = 0 											*/
		  |CAN_CTRL1_SMP(1); 		/* PSEG2 = Phase_Seg2 - 1 = 4 - 1 = 3 							*/
								            /* PSEG1 = PSEG2 = 3 											*/
									/* PROPSEG= Prop_Seg - 1 = 7 - 1 = 6 							*/
									/* RJW: since Phase_Seg2 >=4, RJW+1=4 so RJW=3. 				*/
									/* SMP = 1: use 3 bits per CAN sample 							*/
									/* CLKsrc=0 (unchanged): Fcanclk= Fosc= 8 MHz 					*/

  for(i=0; i<128; i++ )
  {   					/* CAN0: clear 32 msg bufs x 4 words/msg buf = 128 words */
    CAN0->RAMn[i] = 0;  /* Clear msg buf word */
  }
  /**** SHOULD WE DO the BELOW initialization, to start the transfers as IDLE/transmit command*/
  /*Mark Message buffers 0-3 as transfer message buffer*/
  CAN0->RAMn[ 0*MSG_BUF_SIZE + 0] = 0x08000000;
  CAN0->RAMn[ 1*MSG_BUF_SIZE + 0] = 0x08000000;
  CAN0->RAMn[ 2*MSG_BUF_SIZE + 0] = 0x08000000;
  CAN0->RAMn[ 3*MSG_BUF_SIZE + 0] = 0x08000000;



  for(i=0; i<16; i++ )
  {          						/* In FRZ mode, init CAN0 16 msg buf filters */
    CAN0->RXIMR[i] = 0xFFFFFFFF;  	/* Check all ID bits for incoming messages */
  }
  CAN0->RXMGMASK = 0x1FFFFFFF;  				/* Global acceptance mask: check all ID bits 	*/
  CAN0->RAMn[ 4*MSG_BUF_SIZE + 0] = 0x04000000; /* Msg Buf 4, word 0: Enable for reception 	*/
                                                /* EDL,BRS,ESI=0: CANFD not used 				*/
                                                /* CODE=4: MB set to RX inactive 				*/
                                                /* IDE=0: Standard ID 							*/
                                                /* SRR, RTR, TIME STAMP = 0: not applicable 	*/
#ifdef NODE_A                                   /* Node A receives msg with std ID 0x511 		*/
  CAN0->RAMn[ 4*MSG_BUF_SIZE + 1] = 0x14440000; /* Msg Buf 4, word 1: Standard ID = 0x111 		*/
#else                                           /* Node B to receive msg with std ID 0x555 	*/
  CAN0->RAMn[ 4*MSG_BUF_SIZE + 1] = 0x15540000; /* Msg Buf 4, word 1: Standard ID = 0x555 		*/
#endif
                                /* PRIO = 0: CANFD not used */
  CAN0->MCR = 0x0000001F;       /* Negate FlexCAN 1 halt state for 32 MBs */

  while ((CAN0->MCR && CAN_MCR_FRZACK_MASK) >> CAN_MCR_FRZACK_SHIFT)  {}
  /* Good practice: wait for FRZACK to clear (not in freeze mode) */

  while ((CAN0->MCR && CAN_MCR_NOTRDY_MASK) >> CAN_MCR_NOTRDY_SHIFT)  {}
  /* Good practice: wait for NOTRDY to clear (module ready) */
}

void FLEXCAN0_transmit_msg(void)
{
	static ping_pong = 0;
	int nop_loop = 5;
	if (!ping_pong) {
		CAN0->IFLAG1 = 0x00000001;
		//use 0th Message Buffer
		if (CAN0->RAMn[ 0*MSG_BUF_SIZE + 0] == 0x08000000) {
			//Its free so do transfer
			CAN0->RAMn[ 0*MSG_BUF_SIZE + 2] = 0xA5112233;	/* MB0 word 2: data word 0 */
			CAN0->RAMn[ 0*MSG_BUF_SIZE + 3] = 0x44556677; /* MB0 word 3: data word 1 */
			CAN0->RAMn[ 0*MSG_BUF_SIZE + 1] = 0x15540000; /* MB0 word 1: Tx msg with STD ID 0x555 */
			CAN0->RAMn[ 0 *MSG_BUF_SIZE + 0] = 0x0C400000 | 8 << CAN_WMBn_CS_DLC_SHIFT;

		} else {
			//Abort the transfer and try again
			CAN0->RAMn[ 0*MSG_BUF_SIZE + 0] == 0x09000000;
			//Lets give a slight delay
			while(nop_loop--);

			CAN0->RAMn[ 0*MSG_BUF_SIZE + 2] = 0xA5112233;	/* MB0 word 2: data word 0 */
			CAN0->RAMn[ 0*MSG_BUF_SIZE + 3] = 0x44556677; /* MB0 word 3: data word 1 */
			CAN0->RAMn[ 0*MSG_BUF_SIZE + 1] = 0x15540000; /* MB0 word 1: Tx msg with STD ID 0x555 */
			CAN0->RAMn[ 0 *MSG_BUF_SIZE + 0] = 0x0C400000 | 8 << CAN_WMBn_CS_DLC_SHIFT;

		}
		ping_pong = 0;

	} else {
		//use 1st Message Buffer
		CAN0->IFLAG1 = 0x00000002;
		if (CAN0->RAMn[ 1*MSG_BUF_SIZE + 0] == 0x08000000) {
			//Its free so do transfer
			CAN0->RAMn[ 1*MSG_BUF_SIZE + 2] = 0xA5112233;	/* MB0 word 2: data word 0 */
			CAN0->RAMn[ 1*MSG_BUF_SIZE + 3] = 0x44556677; /* MB0 word 3: data word 1 */
			CAN0->RAMn[ 1*MSG_BUF_SIZE + 1] = 0x15540000; /* MB0 word 1: Tx msg with STD ID 0x555 */
			CAN0->RAMn[ 1 *MSG_BUF_SIZE + 0] = 0x0C400000 | 8 << CAN_WMBn_CS_DLC_SHIFT;

		} else {
			//Abort the transfer and try again
			CAN0->RAMn[ 1*MSG_BUF_SIZE + 0] == 0x09000000;
			//Lets give a slight delay
			while(nop_loop--);
			CAN0->RAMn[ 1*MSG_BUF_SIZE + 2] = 0xA5112233;	/* MB0 word 2: data word 0 */
			CAN0->RAMn[ 1*MSG_BUF_SIZE + 3] = 0x44556677; /* MB0 word 3: data word 1 */
			CAN0->RAMn[ 1*MSG_BUF_SIZE + 1] = 0x15540000; /* MB0 word 1: Tx msg with STD ID 0x555 */
			CAN0->RAMn[ 1 *MSG_BUF_SIZE + 0] = 0x0C400000 | 8 << CAN_WMBn_CS_DLC_SHIFT;

		}
		ping_pong = 1;
	}

#if 0
	/*! Assumption:
	 * =================================
	 * Message buffer CODE is INACTIVE
	 */
	CAN0->IFLAG1 = 0x00000001;	/* Clear CAN 0 MB 0 flag without clearing others*/

  CAN0->RAMn[ 0*MSG_BUF_SIZE + 2] = 0xA5112233;	/* MB0 word 2: data word 0 */
  CAN0->RAMn[ 0*MSG_BUF_SIZE + 3] = 0x44556677; /* MB0 word 3: data word 1 */
#ifdef NODE_A
  CAN0->RAMn[ 0*MSG_BUF_SIZE + 1] = 0x15540000; /* MB0 word 1: Tx msg with STD ID 0x555 */
#else
  CAN0->RAMn[ 0*MSG_BUF_SIZE + 1] = 0x14440000; /* MB0 word 1: Tx msg with STD ID 0x511 */
#endif
  CAN0->RAMn[ 0*MSG_BUF_SIZE + 0] = 0x0C400000 | 8 << CAN_WMBn_CS_DLC_SHIFT;
  	  	  	  	  	  	  	  	  	  	  	  	/* MB0 word 0: 								*/
                                                /* EDL,BRS,ESI=0: CANFD not used 				*/
                                                /* CODE=0xC: Activate msg buf to transmit 		*/
                                                /* IDE=0: Standard ID 							*/
                                                /* SRR=1 Tx frame (not req'd for std ID) 		*/
                                                /* RTR = 0: data, not remote tx request frame	*/
                                                /* DLC = 8 bytes 								*/
#endif
}

void FLEXCAN0_receive_msg(void)
{
/*! Receive msg from ID 0x556 using msg buffer 4
 * =============================================
 */
  uint8_t j;
  uint32_t dummy;

  RxCODE   = (CAN0->RAMn[ 4*MSG_BUF_SIZE + 0] & 0x07000000) >> 24;	/* Read CODE field */
  RxID     = (CAN0->RAMn[ 4*MSG_BUF_SIZE + 1] & CAN_WMBn_ID_ID_MASK)  >> CAN_WMBn_ID_ID_SHIFT;	/* Read ID 			*/
  RxLENGTH = (CAN0->RAMn[ 4*MSG_BUF_SIZE + 0] & CAN_WMBn_CS_DLC_MASK) >> CAN_WMBn_CS_DLC_SHIFT;	/* Read Message Length */

  for (j=0; j<2; j++)
  {  /* Read two words of data (8 bytes) */
    RxDATA[j] = CAN0->RAMn[ 4*MSG_BUF_SIZE + 2 + j];
  }
  RxTIMESTAMP = (CAN0->RAMn[ 0*MSG_BUF_SIZE + 0] & 0x000FFFF);
  dummy = CAN0->TIMER;             /* Read TIMER to unlock message buffers */
  CAN0->IFLAG1 = 0x00000010;       /* Clear CAN 0 MB 4 flag without clearing others*/
}

 

 

0 Kudos
Reply
1 Solution
1,266 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

during module initialization it does not matter if CODE 0000b or 1000b is used. Both keeps MB inactive and that MB does not participate neither in matching nor arbitration process.
Commonly clearing whole CS word is used.

Abort is used in situation when prepared message from MB cannot be transmitted for some reason (error detected, heavy bus loading, ...) and you need to stop pending transmission and use this MB for preparation of new message. It is not needed to use it each time message is preparing. In your code EAN bit is cleared so abort is disabled at all.

Generally you should rely on MB flag, which is indication MB was successfully transmitted without error. After successful transmission, the CODE field is changed accordingly (obviously DATA->INACTIVE) and MB flag is set. At that time you can use this MB and prepare new message for transmission.

BR, Petr

View solution in original post

1 Reply
1,267 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

during module initialization it does not matter if CODE 0000b or 1000b is used. Both keeps MB inactive and that MB does not participate neither in matching nor arbitration process.
Commonly clearing whole CS word is used.

Abort is used in situation when prepared message from MB cannot be transmitted for some reason (error detected, heavy bus loading, ...) and you need to stop pending transmission and use this MB for preparation of new message. It is not needed to use it each time message is preparing. In your code EAN bit is cleared so abort is disabled at all.

Generally you should rely on MB flag, which is indication MB was successfully transmitted without error. After successful transmission, the CODE field is changed accordingly (obviously DATA->INACTIVE) and MB flag is set. At that time you can use this MB and prepare new message for transmission.

BR, Petr