Hi, I am trying to connect TI DP83848 ethernet phy to evaluation board using RMII. I am using lwIP demo to test that the hardware is working so i can work on the PCB.
S32 SDK says:
S32 SDK: lwIP TCP/IP stack
The following boards are supported by this application:
S32K148EVB-Q100
I am using 176 pin version. What would be the difference? Pinout?
Do i need to make modifications to the evaluation board?
Thanks,
Jani
Tested with enet loopback demo, and started seeing signal at TX pins. Something wrong with the phy though, its only transmitting 1.2V RX signals, and they are not getting through level shifter.
These cheap module boards are pretty bad and wiring 50Mhz signals with dupont wires is not the best idea either, getting so much noise...
I am feeling cofinent enough, going make the PCB. :smileyhappy:
Hi Jani,
the pins - in meaning pin names - are same for Ethernet across all package layouts:
Example itself is tested with TJA1100 Ethernet phy. You need to change package layout in project to 176 pins:
https://community.nxp.com/docs/DOC-334936
Hope it helps.
Jiri
Hi, I cannot get this to work.
I am using ethernet board with schematic like this:
https://www.waveshare.com/w/upload/3/31/DP83848-Ethernet-Board-Schematic.pdf
I made breakout board for the QTH connector J16, and connected the board with dupont wires.
Connections seem to be OK, checked everything with multimeter, nothing shorted or unconnected.
I have RMII wired like this:
phy pin-mcu pin, pin in evb J16
-------------------------
TXD0-PTC2, PIN 14
TXD1-PTD7, PIN 16
TXEN-PTD12, PIN 24
OSCIN/X1-PTD11, PIN 20
CRSDV-PTC17, PIN 28
RX0-PTC1, PIN 36
RX1-PTC0, PIN 38
MDIO-PTB4,PIN 48
MDC-PTB5, PIN 50
Note, Receive error not connected
I am using LwIP example with prosessor changed to 176 pin version. Code is running just fine.
When i tested with oscilloscope, i saw <1V signal in TX0 and TX1 pins at MCU. Why does it not get to 5V?
I looked reference manual and it says on page 1845:
Enable the Drive strength for the transmitting pads of ENET by setting DSE field of PORT_PCRn register
LwIP example does not seem to do that. I tried to modify the generated pin mux to do that:
TX Signals still not getting pulled to 5V.
Can anyone help?