S32K148 ISR not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K148 ISR not working

2,329 次查看
satish_k_singh
Contributor III

Hello ,

I am trying to write an ISR routine  on s32k148 eval board  and would want  that it  detects the switch (PTC 13 on rising edge) and toggle the output  BLUE LED (PORTE 23), but I see the blue LED glowing but the Interrupt is not getting detected when the SW4 is pressed.

So could you please let know if I have missed something.

The below is the sample code.

Config from the  processor expert.

{
.base = PORTC,
.pinPortIdx = 12u,
.pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED,
.passiveFilter = false,
.driveSelect = PORT_LOW_DRIVE_STRENGTH,
.mux = PORT_MUX_AS_GPIO,
.pinLock = false,
.intConfig = PORT_INT_RISING_EDGE,
.clearIntFlag = true,
.gpioBase = PTC,
.direction = GPIO_INPUT_DIRECTION,
},

{
.base = PORTE,
.pinPortIdx = 23u,
.pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED,
.passiveFilter = false,
.driveSelect = PORT_LOW_DRIVE_STRENGTH,
.mux = PORT_MUX_AS_GPIO,
.pinLock = false,
.intConfig = PORT_DMA_INT_DISABLED,
.clearIntFlag = false,
.gpioBase = PTE,
.direction = GPIO_OUTPUT_DIRECTION,
},

void FS0B_ISR(void)

{
PINS_DRV_ClearPinIntFlagCmd(PORTC, (1<<13));
PINS_DRV_TogglePins(PTE, (1<<23));

}

main()

{

CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);
PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);


PINS_DRV_SetPinDirection(PTC, (1<<13), 0);
PINS_DRV_SetPins(PTE, (1<<23));
INT_SYS_InstallHandler(PORTC_IRQn, FS0B_ISR, (isr_t *)0);
INT_SYS_EnableIRQ(PORTC_IRQn);
PINS_DRV_SetPinIntSel(PORTC,(1<<13),PORT_INT_RISING_EDGE);

}

标记 (4)
0 项奖励
回复
1 回复

2,067 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

here is simple example for GPIO Interrupt handler - https://community.nxp.com/docs/DOC-343587 

Hope it helps. 

Jiri