S32K146 Variant handling

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K146 Variant handling

1,321件の閲覧回数
S32k1
Contributor I

Hi Team,

I need to know is it possible to switch between the ResourceSubderivative value according to the change in variant change that is like when i change the variant to 64pins does the value in the resource tab get automatically switch to s32k146_lqfp64 and to s32k146_lqfp100 when i change the variant to 100pins.

Thank you

0 件の賞賛
返信
3 返答(返信)

1,253件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @S32k1 

Yes, you can change the package or derivative in Resource. But some reconfigurations may be required. You can take a look at this thread:

https://community.nxp.com/t5/S32K/Autosar-MCAL-Template-Application-for-S32K142/m-p/1234165

Regards,

Lukas

0 件の賞賛
返信

1,242件の閲覧回数
S32k1
Contributor I

Hi @lukaszadrapa ,

Sorry for your misunderstanding, let me clear again. 

I have 2 variants which contain 64pins and 100pins like min-variant and max-variant respectively. So if I want to switch between variants in EB like changing the variant from min to max will the value in the resource container also changes along with it (when change from 64pin to 100pins) also does the MCAL config changes according to that board.

Is this possible?

Note: Here only the pin numbers are different, but the family is same s32k146 (64 and 100pins)

Thanks

0 件の賞賛
返信

1,208件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @S32k1 

No, the configurator won't automatically update your project. It's up to user. The configurator will just show a list of errors. For example, if you are going from large derivative to smaller one, it will notify you that some pins are not available in that package or that some peripheral instance is not there...

Regards,

Lukas

0 件の賞賛
返信