S32K Chip Performance and Motor Control

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K Chip Performance and Motor Control

跳至解决方案
1,361 次查看
zhangchun
Contributor III

hello

I am currently using s32k144 to create a motor controller, but due to the performance impact of s32k144, the motor controller cannot achieve the expected state.

At present, I have used a system frequency of 80M in my code, with O3 as the optimization level, cache enabled, FPU enabled, and fixed-point operations used to improve code execution efficiency.

I want to replace a chip without changing the current code to improve performance, and choose a chip with a higher system frequency and larger cache, among other factors.

excuse me

1. Are there any other optimization plans to improve code performance

2. Do the s32k series chips have the same IP addresses as S32K144's FTM, TRGMUX, PDB, ADC, and have higher performance?

 

Thanks!

标记 (1)
0 项奖励
回复
1 解答
1,317 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you tried to use AMMClib? This library is very well optimized for motor control. 

jiri_kral_0-1693488234372.png

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,318 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you tried to use AMMClib? This library is very well optimized for motor control. 

jiri_kral_0-1693488234372.png

 

0 项奖励
回复
1,310 次查看
zhangchun
Contributor III
Hi
Thank you very much for your reply,
0 项奖励
回复