S32G2: S32DS: Cannot open the Configuration Tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G2: S32DS: Cannot open the Configuration Tool

ソリューションへジャンプ
5,023件の閲覧回数
Keita_Nagashima
NXP Employee
NXP Employee

Hi Sir or Madam,

I installed necessary packages into S32DS, and imported some example projects.

KeitaNaga_1-1647313925418.png

Some projects can be installed into my environment, but the .mek file for Configuration Tool cannot be opened.

KeitaNaga_2-1647314392744.png

 

This issue appears to depend on PlatformSDK version, but I couldn't understand the version dependence.

 

Would you tell me the how to solve this issue? 

I would also like to know about the Version dependency with PlatformSDK.

 

Best Regards,

Keita

 

 

0 件の賞賛
返信
1 解決策
5,009件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Keita,

It seems this project is quite old and was created for the RTD which was released in December 2020. I suggest you use the new version which was included in the updated RTD you installed.

image.png

Best Regards,

Mike

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
5,010件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Keita,

It seems this project is quite old and was created for the RTD which was released in December 2020. I suggest you use the new version which was included in the updated RTD you installed.

image.png

Best Regards,

Mike

0 件の賞賛
返信
4,999件の閲覧回数
Keita_Nagashima
NXP Employee
NXP Employee

@mikedoidge ,

 

Thank you for your reply. I understood it.

BTW, do you know how to delete the old project like December 2020 version?

I'd like to manage the all project.

 

Best Regards,

Keita

0 件の賞賛
返信
4,984件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Keita,

To remove the old examples, you would need to uninstall the old RTD. Probably it is the 2.0.0 version.

image.png

 

0 件の賞賛
返信
4,977件の閲覧回数
Keita_Nagashima
NXP Employee
NXP Employee

Hi @mikedoidge ,

Thank you for your reply.

Please refer to the figure in my original message. I have already deleted the old RTD and my environment was not seen it.

But, the old version of the sample programs are still there...

 

Best Regards,

Keita

0 件の賞賛
返信
4,946件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

If the old version of the RTD was uninstalled from S32 Design Studio, then the associated example projects should be removed as part of that process.

Perhaps check the following directories to see if some content from the old RTD is left behind:

C:\NXP\S32DS.3.4\S32DS\integration

C:\NXP\S32DS.3.4\S32DS\software

Best Regards,

Mike

0 件の賞賛
返信
4,892件の閲覧回数
Keita_Nagashima
NXP Employee
NXP Employee

Hi @mikedoidge ,

 

Sorry for my delay response.

Yes, I was able to remove old sample codes by deleting the old files manually.

 

Best Regards,

Keita

0 件の賞賛
返信