S32G2 : MCU is not supported

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G2 : MCU is not supported

Jump to solution
4,452 Views
yonghwi_lee
NXP Employee
NXP Employee

Hi Team,

Our custoemr, HL Mando, has reported that S32DS shows "MCU is not supported" and customer can not generate source code by Configuration Tool.

yonghwi_lee_0-1687855928693.png

yonghwi_lee_1-1687855941722.png

Customer installed below packages

S32DS.3.4_b201217_win32.x86_64.exe
SW32G_S32DS_3.4.3_D2112.zip
SW32G_RTD_4.4_3.0.2_HF01_DS_updatesite_D2204.zip
SW32G_IPCF_4.6.0_D2205_updatesite.zip

Could let me know why this error shows and how to solve this issue?

Best regards,
Yonghwi Lee

Labels (2)
0 Kudos
Reply
1 Solution
4,254 Views
yonghwi_lee
NXP Employee
NXP Employee

Hi Mehul,

Customer found the solution after investigating ".metadata\.log ". 

The log showed "Could not parse file 'C:\NXP\S32DS.3.4_1\eclipse\mcu_data\processors\S32G274A_Rev2\PlatformSDK_S32XX_2022_03\clocks\S32V2xx.dsn" and S32V2xx.dsn was encrypted via DRM.

The customer security program prevented S32V2xx.dsn from parsing. Some security rules were changed in customer site and problem solved.

Thanks for your supports.

Best regards,
Yonghwi Lee

View solution in original post

9 Replies
3,798 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

@Changwoo82 , 

 

Thank you for comment on the issue. 

 

Happy coding. 

- Mehul Patel 

0 Kudos
Reply
4,285 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @yonghwi_lee , 

Sorry for the late reply,

Please can you ask customer to send workspace log from 

C:\Users\Public\[Workspace]\.metadata to help if there is any error. (or wherever the particular workspace is located from that workspace log)

Thank you. 

- Mehul

0 Kudos
Reply
4,295 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @yonghwi_lee , 

Sorry for the late reply. 

Please can you ask the customer for the workspace log, which should be available at 

C:\Users\Public\[Workspace name]\.metadata

Thank you, Best regards, 

- Mehul Patel

0 Kudos
Reply
4,255 Views
yonghwi_lee
NXP Employee
NXP Employee

Hi Mehul,

Customer found the solution after investigating ".metadata\.log ". 

The log showed "Could not parse file 'C:\NXP\S32DS.3.4_1\eclipse\mcu_data\processors\S32G274A_Rev2\PlatformSDK_S32XX_2022_03\clocks\S32V2xx.dsn" and S32V2xx.dsn was encrypted via DRM.

The customer security program prevented S32V2xx.dsn from parsing. Some security rules were changed in customer site and problem solved.

Thanks for your supports.

Best regards,
Yonghwi Lee

4,291 Views
yonghwi_lee
NXP Employee
NXP Employee

Hi Mehul,

Project shows below errors.

yonghwi_lee_0-1688981251038.png

 

An error has occurred. See error log for more details.

PeripheralExpressionException[

Description: Could not parse string argument: "" to rational number

Function: toInt(valid)

Contexts:

ExpressionContext[ child_context = ChildContext[

$this = Mcu.McuModuleConfiguration.McuClockSettingConfig.0.McuRtcClockSelect.McuRtc_Source

$instance = Mcu

$group = BOARD_InitPeripherals]]

 

ExpressionContext[ child_context = ChildContext[

$this = Mcu.McuModuleConfiguration.McuClockSettingConfig.0.McuRtcClockSelect.McuRtc_Source

$instance = Mcu

$group = BOARD_InitPeripherals]]

 

ExpressionContext[ child_context = ChildContext[

$this = Mcu.McuModuleConfiguration.McuClockSettingConfig.0.McuRtcClockSelect.McuRtc_Source

$instance = Mcu

$group = BOARD_InitPeripherals]]

 

ExpressionContext[ child_context = ChildContext[

$this = Mcu.McuModuleConfiguration.McuClockSettingConfig.0.McuRtcClockSelect.McuRtc_Source

$instance = Mcu

$group = BOARD_InitPeripherals]]

]

 

I will ask for customer to get metadata.

Best Regards,
Yonghwi Lee

4,422 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @yonghwi_lee , 
Please can you get more information from the customer to understand the issue. 

Or, please can you suggest the customer to use S32DS3.5 and the latest package for S32G2 required for it.  

Thank you, Kind regards. 

- Mehul

0 Kudos
Reply
4,326 Views
yonghwi_lee
NXP Employee
NXP Employee
Hi Mehul,

The customer installed security program on windows. I think this issue is casued by security program.
The customer needs to solve this issue to use S32D2 and asked what could be causing this issue and how to get error logs.
Could you let me know the details of the error "MCU is not supported"?

Best regards,
Yonghwi Lee
0 Kudos
Reply
4,362 Views
yonghwi_lee
NXP Employee
NXP Employee
Hi Mehul,

The customer alreday installed the latest package for S32G2 and it still shows same error "MCU is not supported". I did test S32G2 package and I can't reproduce this issue.

Could you let me know what could be causing this issue and is there something to get error logs?

Best regards,
Yonghwi Lee
0 Kudos
Reply
3,870 Views
Changwoo82
Contributor II

I believe the issue has already been resolved, but I wanted to leave this comment here.

I encountered the same problem, and it was resolved after decrypting the file 'S32V2xx.dsn.