S32G RTD errors in S32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G RTD errors in S32DS

ソリューションへジャンプ
5,455件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

Hello there,

I got some errors when created an S32G RTD configuration project in S32DS.

these errors show that peripherals drivers are not found in toolchain/IDE project.

see attached image.

any suggestion?

Many thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
5,442件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

the problem solved.

right click error and then "add ..." will solve the issue.

元の投稿で解決策を見る

4 返答(返信)
4,743件の閲覧回数
murphy_xie
Contributor I

Hi nxp

     when I trying to install RTD as  S32 Design Studio v3.4.1及RTD 2.0.0 HF4安装指南_v20210810.pdf 

,but I can not find RTD package for S32G2,only S32K1 and S32k3 valueable,can you help to solve it,tks.
0 件の賞賛
返信
4,738件の閲覧回数
Rick_Li
NXP Employee
NXP Employee
0 件の賞賛
返信
4,725件の閲覧回数
murphy_xie
Contributor I

Hi Rick

   tks,it working.

B.R

 

0 件の賞賛
返信
5,443件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

the problem solved.

right click error and then "add ..." will solve the issue.