S32G-PROCEVB-S (S32G274A) DDR Tool Failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G-PROCEVB-S (S32G274A) DDR Tool Failure

1,149 Views
bishoy_rafaiel
Contributor II

I'm currently trying the DDR tool in the S32 Design studio using the evaluation board "S32G-PROCEVB-S" with the following extensions installed:

Package: NXP GCC for Arm Embedded Processors v9.2 build 1627; Version: 1627; Build id: 202003031402
Package: S32 Design Studio Platform Tools package; Version: 3.2.2; Build id: 202004222055
Package: S32G2xx development package; Version: 3.2.2; Build id: 202004222145
Package: S32SDK S32G274 BETA 0.9.0; Version: 0.9.0; Build id: 202003261626
Package: S32 Design Studio Platform package; Version: 3.2.2; Build id: 202004222055
Package: NXP GCC for Arm Embedded Processors Build 1574; Version: 1574; Build id: 201909041333
Package: NXP GCC for Arm Embedded Processors Build 1620; Version: 1620; Build id: 201909041409

The problem is that it stucks upon the execution in a state called "APP_WAIT_FOR_INPUT" where it read the value "AA55AA55" continously without ending the execution and without generating the code as well.

I've treid this with SDK S32SDK S32G274 BETA 0.9.0; and with S32SDK S32G274 EAR 0.8.0; as well

Also I've tried with the serial and with the S32 Debug probe and I get the same result in both

Attached below the debug log of the execution so I'd appreciate someone can pin-point where the problem is, Is there any switch or jumper configuration that need to be done on the evaluation board  itself or there's something wrong with the S32DS configuration.

0 Kudos
0 Replies