S32DesignStudio command line tool or configuration tool usage documentation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DesignStudio command line tool or configuration tool usage documentation

1,597 次查看
Jackey_cj
Contributor I

hello,

 

I want to add a step in the build process to switch configuration sets in the process of automating unit tests. I wondered if I could do this by calling the S32K configuration tool or the command line tool, but when I looked for the relevant documentation, I couldn't find anything that contained the relevant content.

0 项奖励
回复
4 回复数

1,545 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

what's your S32DS version and target device? 

0 项奖励
回复

1,477 次查看
Jackey_cj
Contributor I

hi,

 Is there any data on that?

0 项奖励
回复

1,399 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

I'm not sure what you mean by configuration - If you like build for example only Debug_FLASH target, you can add /Debug_FLASH (or the configuration name in your project) after project name. Like this. 

c:\NXP\S32DS_ARM_v2.2\eclipse\s32ds.exe -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild --launcher.ini c:\S32DS_ARM_v2.2\eclipse\s32ds.ini -data c:\users\user\workspaceS32DS.ARM.2.2 -cleanBuild hello_world_s32k144/Debug_FLASH

 

0 项奖励
回复

1,539 次查看
Jackey_cj
Contributor I

S32DS ARM 2.2 & S32DS POWER 2.1

MPC5745B  & S32K146

0 项奖励
回复