S32DS3.6 Cannot find S32K1xx SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS3.6 Cannot find S32K1xx SDK

ソリューションへジャンプ
945件の閲覧回数
Solon
Contributor I

Hi, I can not find S32K1xx SDK/RTD package in S32DS Extensions and Updates.

Where should I look for it ?

Thanks!

ラベル(1)
0 件の賞賛
返信
1 解決策
937件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please offline install S32K1 RTD by refer to the step 4 of HOWTO: offline install S32K1 RTD 2.0.0 in S32DS v3.5.

I installed the latest S32K1 RTD 2.0.0 QLP1 in S32DS v3.6.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
938件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please offline install S32K1 RTD by refer to the step 4 of HOWTO: offline install S32K1 RTD 2.0.0 in S32DS v3.5.

I installed the latest S32K1 RTD 2.0.0 QLP1 in S32DS v3.6.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

927件の閲覧回数
Solon
Contributor I
Thanks!
0 件の賞賛
返信