S32DS3.4_the SDK of K144 Issue_FC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS3.4_the SDK of K144 Issue_FC

Jump to solution
2,183 Views
Fidel
Contributor IV

Dears,

      I am using S32DS3.4 to develop K144, and I want to make a new project using "File->New->S32DS Application Project", but when I choose the SDK, I cannot find the standard SDK for K1(such as "S32K1xx RTM SDK.....", although I have installed it by the related  " .exe" file downloaded from NXP offical website ), detailed picture as below, the only 2 sdks shown are "AMMCLIB_S32K14x" and "FreeMaster_S32K144",please tell me how to resolve it? thx!

Fidel_0-1668828036627.png

 

0 Kudos
Reply
1 Solution
2,161 Views
jiri_kral
NXP Employee
NXP Employee

Hi,

yes, SDK is built with gcc v6.3. If you choose higher version, SDK is not available. 

View solution in original post

0 Kudos
Reply
4 Replies
2,164 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

do you have installed S32K1xx SDK package? 

jiri_kral_0-1669289035185.png

 

If So, please make sure that you choose correct toolchain in New Project Wizard (gcc v6.3):

jiri_kral_1-1669289160495.png

 

 

0 Kudos
Reply
2,163 Views
Fidel
Contributor IV

if the tool chain is wrong ,then the SDK cannot be found in the next page?

0 Kudos
Reply
2,162 Views
jiri_kral
NXP Employee
NXP Employee

Hi,

yes, SDK is built with gcc v6.3. If you choose higher version, SDK is not available. 

0 Kudos
Reply
2,159 Views
Fidel
Contributor IV

hi Jiri,

        I checked what you said , and just like you said , with different GCC version ,different SDK showed up, thanks a lot~

 

0 Kudos
Reply