S32DS3.4 and S32DS3.5 can be installed in the same PC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS3.4 and S32DS3.5 can be installed in the same PC?

2,186件の閲覧回数
phidiawang
Contributor III

Hi,

S32DS3.4 and S32DS3.5 can be installed in the same PC? 

I have installed S32DS3.5 in my PC,now i wanna intall S32DS3.4 in it,but it show a error:the activation code is used by s32ds3.5. How can i install the two version? thanks.

3d51f4a3027ebd1a2d84fdebed0f768.jpg

0 件の賞賛
返信
4 返答(返信)

2,170件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

you are probably using wrong activation key. What is the key used for activation of S3DS v3.4?

 

Jiri

0 件の賞賛
返信

2,163件の閲覧回数
phidiawang
Contributor III

Hi,

Activation Code: 0A85-E852-148E-082D ,I used this activation code to successfully install S32DS3.4 last month,but this week i uninstalled  S32DS3.4 and successfully installed S32DS3.5 (used this activation code). Now,I wanna install S32DS3.4 and 3.5 in the same PC. please help,thanks.

0 件の賞賛
返信

2,153件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello,

It seems the activation code you are using (0A85-E852-148E-082D) has been migrated to work for S32DS 3.5, so now it cannot be used for S32DS 3.4. For S32DS 3.4, you should use the activation code you have on your account for the S32DS 3.4, CBE1-1765-9C4C-C004.

Best Regards,

Mike

0 件の賞賛
返信

2,135件の閲覧回数
phidiawang
Contributor III

Hi,

thanks a lot,I have installed S32DS3.4.

0 件の賞賛
返信