S32DS3.4 and S32DS3.5 can be installed in the same PC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS3.4 and S32DS3.5 can be installed in the same PC?

2,216 Views
phidiawang
Contributor III

Hi,

S32DS3.4 and S32DS3.5 can be installed in the same PC? 

I have installed S32DS3.5 in my PC,now i wanna intall S32DS3.4 in it,but it show a error:the activation code is used by s32ds3.5. How can i install the two version? thanks.

3d51f4a3027ebd1a2d84fdebed0f768.jpg

0 Kudos
Reply
4 Replies

2,200 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

you are probably using wrong activation key. What is the key used for activation of S3DS v3.4?

 

Jiri

0 Kudos
Reply

2,193 Views
phidiawang
Contributor III

Hi,

Activation Code: 0A85-E852-148E-082D ,I used this activation code to successfully install S32DS3.4 last month,but this week i uninstalled  S32DS3.4 and successfully installed S32DS3.5 (used this activation code). Now,I wanna install S32DS3.4 and 3.5 in the same PC. please help,thanks.

0 Kudos
Reply

2,183 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

It seems the activation code you are using (0A85-E852-148E-082D) has been migrated to work for S32DS 3.5, so now it cannot be used for S32DS 3.4. For S32DS 3.4, you should use the activation code you have on your account for the S32DS 3.4, CBE1-1765-9C4C-C004.

Best Regards,

Mike

0 Kudos
Reply

2,165 Views
phidiawang
Contributor III

Hi,

thanks a lot,I have installed S32DS3.4.

0 Kudos
Reply