S32DS issue after update?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS issue after update?

1,810件の閲覧回数
mschroeder
Contributor I

Today morning S32DS_POWER_2017.R1 was working fine. I allowed some updates to be installed, but after restarting S32DS it now stops during "Loading com.freescale.processorexpert.core" (see attachment). I could "fix this by moving away all fresh files & folders with todays date from C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins. Afterwards S32DS is working again.

Does anybody encounter the same problem? My system is a fully patched Windows 7 64-Bit.

ラベル(1)
0 件の賞賛
返信
1 返信

1,545件の閲覧回数
mschroeder
Contributor I

Well, after removing S32DS and a fresh install I got the same problem even without the latest update S32DS_PA_2017_R1_UP1. So I could track this problem down to my workspace.

0 件の賞賛
返信