S32DS for vision v2.0 build error(import sdk from vsdk)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS for vision v2.0 build error(import sdk from vsdk)

887件の閲覧回数
huangtianxiang
Contributor I

Hi,

      It's my first-time use S32DS for vision, I refer the Release note:

pastedImage_1.png

I have copied the SDK folder to S32ds install folder.

However, when I import the sample project(e.g. isp_sonyimx224_csi_dcu) and build it, there are 2 problems I can't fix. 

The first problem is the OSDIR is not defined.

pastedImage_3.png

After I modified the OSDIR to "linux" there is a new problem.

pastedImage_2.png

Is there anyone has the same problem, Thanks.

My PC environment is:

Win10_64bit

S32DS for vision newest one.

ラベル(2)
タグ(2)
0 件の賞賛
返信
0 返答(返信)