S32DS for S32 v3.5 Update failed issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS for S32 v3.5 Update failed issue

Jump to solution
2,600 Views
ssean
Contributor IV

Hello.

Step 1. I install S32DS for S32 v3.5.

- Install program: S32DS.3.5_b220726_win32.x86_64.exe 

Step 2. Select "S32 Design Studio Platform package" and execute update.

Step 3. After few minute update failed with "Read time out" error.

Step 4. Close & Restart S32DS, and retry update "S32 Design Studio Platform package".

Step 5. S32DS program close suddenly. And s32ds.exe, s32ds.bat file deteled.

I attached my step screen capture below.

 

How can I clean install S32DS for S32 v3.5 and update latest package?

 

Best Regards,

Sean Sung

 

ssean_0-1728537525540.png

ssean_1-1728537802216.png

ssean_2-1728537810536.png

ssean_3-1728537818411.pngssean_4-1728537825019.png

ssean_5-1728537836131.png

ssean_6-1728537897178.png

 

Tags (1)
0 Kudos
Reply
1 Solution
2,068 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

on some machines doesn't work repositories with http:// - please try to change http:// to https://

jiri_kral_0-1733412029468.png

 

 

 

View solution in original post

0 Kudos
Reply
6 Replies
2,069 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

on some machines doesn't work repositories with http:// - please try to change http:// to https://

jiri_kral_0-1733412029468.png

 

 

 

0 Kudos
Reply
2,046 Views
ssean
Contributor IV
Thank you for support!
It works.
0 Kudos
Reply
2,581 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Have you tried installing offline? Refer to the step2 of HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5

S32 Design Studio 3.5 Update 13 D2407 is available for download on S32 Design Studio for S32 Platform web page.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,558 Views
ssean
Contributor IV

Hi @Robin_Shen 

I already tried offline update.

Update okay with belows.

SW32_S32DS_3.5.2_D2302, SW32_S32DS_3.5.3_D2306, SW32_S32DS_3.5.4_D2307, SW32_S32DS_3.5.5_D2308, SW32_S32DS_3.5.6_D2309.

ssean_0-1728603388872.png

 

When I try update to SW32_S32DS_3.5.8_D2311, warning message popup.

I choose "Install anyway", after then program close (without any message), and deleted s32ds.exe and s32ds.bat.

ssean_1-1728603425970.png

 

When I try update to latest package SW32K3_S32DS_3.5.13_D2407 at one-shot(without update previous version), same issue happend.

 

And.. I can't find offline update package for Update 7.

ssean_2-1728603582415.png

 

Could you check for me?

 

Best Regards,

Sean Sung.

Tags (1)
0 Kudos
Reply
2,552 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please tell me which version of S32K3 RTD you want to install? Here is the method for offline installation of S32K3 RTD 4.0.0: RTD 4.0 with Design Studio 3.5 

SW32K3_S32DS_3.5.13_D2407.zip is S32 Design Studio 3.5.13 Development Package with support for S32K3xx devices. As far as I know, this only needs to be installed when installing S32K3 RTD 5.0.0.

You don't need to install those S32DS Update packages one by one, just install the latest one. For example: S32 Design Studio 3.5 Update 14 D2409 new

0 Kudos
Reply
2,542 Views
ssean
Contributor IV

Hi @Robin_Shen 

 

When I try offline update to SW32_S32DS_3.5.14_D2409, same issue (deleted .exe, .bat files) happened.

ssean_0-1728611377560.png

ssean_1-1728611382295.png

 

SW32K3_S32DS_3.5.13_D2407.zip is my mistype, I don't need that.

 

Best Regards,

Seam Sung.

0 Kudos
Reply