S32DS for Arm 2.2 activation not possible

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS for Arm 2.2 activation not possible

ソリューションへジャンプ
1,622件の閲覧回数
6T9
Contributor III

Hello,

today I opened my S32DS for Arm 2.2 and I tells me my license is missing.

fedev_0-1700204492036.png

It's a bit weird because I used it yesterday without an issue.

I tried to activate it with my activation code from my NXP Software Account.

But I'm getting the notification: Your Software Activation Code is for another feature. Do you want to return it?

fedev_1-1700204718955.png

The same notification is shown for online and offline activation.

I checked my NXP Software Account it is the correct activation code, it is not expired (expiration date april 2026) and I have plenty available licenses.

Could you please help me?

Best regards

Thomas

0 件の賞賛
返信
1 解決策
1,604件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @6T9 , 

 

Please can you retry the activation for the S32DS for Arm 2.2. 

 

Let us know if you are still facing the issue. 

Thank you. Best regards. 

-Mehul Patel 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,574件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, Thomas,

 

Great that you are able to use S32DS now. 

 

Best regards. 

 

- Mehul Patel 

 

0 件の賞賛
返信
1,605件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @6T9 , 

 

Please can you retry the activation for the S32DS for Arm 2.2. 

 

Let us know if you are still facing the issue. 

Thank you. Best regards. 

-Mehul Patel 

0 件の賞賛
返信
1,581件の閲覧回数
6T9
Contributor III

Hi @Mehul_Patel_NXP ,

 

after retrying the activation for about 8 times it worked.

The whole time I used the same activation code.

I had the same issue with other versions of the S32DS as well.

Could it be there is a problem, when more than one version is installed?

 

Best regards

0 件の賞賛
返信