[S32DS for ARM v2.2] S32K144 Import and Build issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[S32DS for ARM v2.2] S32K144 Import and Build issue

1,021 Views
james-lee
NXP Employee
NXP Employee

Hello team,

 

My customer reported the import & build issue for the S32DS for ARM v2.2.

They tried to import the project which they received from their customer, and faced the issue that the progress was pending at the compiler built-in language setting.

J_W__0-1620802040383.png

 

So they stopped this setting and then the import was done. However, when they tried to build it, the build process was pending at below.

J_W__1-1620802207212.png

 

Would you please give me some advice for the potential root cause and what I should check further?

 

Best regards,

James

0 Kudos
Reply
2 Replies

1,011 Views
jiri_kral
NXP Employee
NXP Employee

Hi James, 

it is first time when I'm seeing such issue. It is possible share customer's project - for example via NXP email? 

 

Jiri

0 Kudos
Reply

974 Views
james-lee
NXP Employee
NXP Employee

Hi Jiri,

 

Thanks for your answer, but customer couldn't share their project because of their s/w security policy.

I shared your answer that we never seen this kind of issue, and let you know if I have further update from customer.

 

Best regards,

James

0 Kudos
Reply