S32DS erases everything in the output folder when building the project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS erases everything in the output folder when building the project

884 次查看
jimd2023
Contributor I

Hi guys, how can I turn off the feature in S32DS that erases everything in the output folder when building the project as I have some files there like the bootloader hex file and the tools that merge the bootloader with the application hex file and it is really not convenient to copy them back every time?

Thanks in advance for the help 

0 项奖励
回复
1 回复

850 次查看
mikedoidge
NXP Employee
NXP Employee

Hello Jim,

If you are referring to the folder 'Debug_RAM', for example, then only the files which are a product of the build are erased and replaced. If you rename the files they should remain in the folder.

What version of S32DS are you using?

Best Regards,

Mike

0 项奖励
回复