S32DS debug error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32DS debug error

跳至解决方案
1,255 次查看
George_Ye
Contributor II

I used to debug with version 3.4.0 normally. Today, after updating with the 3.4.3 update package, an error occurred. Tips "Break at address "0x0" with no debug information available, or outside of program code",how can I do?

My debugger is PE micro.

标签 (1)
0 项奖励
1 解答
913 次查看
George_Ye
Contributor II
配置工具和SDK不配套

在原帖中查看解决方案

0 项奖励
4 回复数
923 次查看
hupengpeng203
Contributor I

我和你有同样的问题。你解决了吗?

0 项奖励
914 次查看
George_Ye
Contributor II
配置工具和SDK不配套
0 项奖励
1,240 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

what's your target MCU? Can you please share output from debug console? What optimization level - is set do none? 

0 项奖励
1,237 次查看
George_Ye
Contributor II

See attach file, thanks.MCU is s32k 314.optimization level is "-Os"(Optimize for size), and setting to none also made no sense.

0 项奖励