S32DS debug error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS debug error

Jump to solution
1,246 Views
George_Ye
Contributor II

I used to debug with version 3.4.0 normally. Today, after updating with the 3.4.3 update package, an error occurred. Tips "Break at address "0x0" with no debug information available, or outside of program code",how can I do?

My debugger is PE micro.

Labels (1)
0 Kudos
1 Solution
904 Views
George_Ye
Contributor II
配置工具和SDK不配套

View solution in original post

0 Kudos
4 Replies
914 Views
hupengpeng203
Contributor I

我和你有同样的问题。你解决了吗?

0 Kudos
905 Views
George_Ye
Contributor II
配置工具和SDK不配套
0 Kudos
1,231 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

what's your target MCU? Can you please share output from debug console? What optimization level - is set do none? 

0 Kudos
1,228 Views
George_Ye
Contributor II

See attach file, thanks.MCU is s32k 314.optimization level is "-Os"(Optimize for size), and setting to none also made no sense.

0 Kudos