S32DS can't find OpenSDA debug port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS can't find OpenSDA debug port

6,827 Views
jiachun_li
Contributor I

I want to use S32DS to debug [S32K144 Evaluation Board], but [P&E Connection Assisant] tells me [No device Available],  please look at the attachment [PE-Err.PNG], I also uploaded an attachment [Dev-info.PNG] for the device information, can anybody give me some help? Thanks.

0 Kudos
Reply
5 Replies

6,363 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

isn't another instance of pegdbserver running? (please check it with Windows task manager and if there is another instance - just end the task). 

Also make sure that you installed all updates - including the PE Micro ones : 

https://community.nxp.com/docs/DOC-342273 

Jiri

0 Kudos
Reply

6,363 Views
aashitole
Contributor I

For me it's not working! :smileysad:

Not able to find the USB port for FRDM-KEAZN32Q64 boardCapture1.PNG

Do we need to select SDKs while creating project?

SDK for FRDM-KEAZN32Q64 are not available.

By default it is showing below options. Which one to choose?

Capture.PNG

0 Kudos
Reply

6,363 Views
stanish
NXP Employee
NXP Employee

Hi,

You don't have to select SDK.

First of all make sure you are using up-to-date Pemicro drivers that fixes a similar issue under Windows 10

(PEmicro | Experts in Embedded tools for Flash Programming and Development)

Please check in Device manager that OpenSDA interface has been detected:

pastedImage_7.png

If it wasn't detected make sure your board is properly powered (green LEDs D2 and D3  are ON).

Hope it helps.

Stan

6,363 Views
aashitole
Contributor I

Now, I can see the USB port.

However getting these errors when I try to load the code/ program the board.

pastedImage_1.png

0 Kudos
Reply

6,363 Views
jiachun_li
Contributor I

Thanks for your reply, by reinstalling the driver, now S32DS can find the debug port.

0 Kudos
Reply