S32DS build problem about MPC5775B project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS build problem about MPC5775B project

Jump to solution
2,853 Views
Tangsheng_Zhou
NXP Employee
NXP Employee

I wrote a test software for MPC5775B. However,  the executable image .elf file could not be generated in the Debug_RAM mode, but it could make it in the Debug mode. Please refer to error message as below:

C:\NXP\S32DS_Power_v2017.R1\Cross_Tools\powerpc-eabivle-4_9\bin\powerpc-eabivle-size.exe: 'a.out': No such file
Finished building: ../Sources/pdc_tasks.c
make: *** [makefile:83: libPDC_5775B_SDK_Example_Z7_0.siz] Error 1
make: *** Waiting for unfinished jobs....

 

pastedImage_1.png

I checked out the Cross Settings properties between Debug_RAM mode and Debug mode of this project, I found something different as below. There is nothing about the powerpc-eabivle-size.exe command in the Debug_RAM mode. I did not find that I could add the command. And Could find the command "powerpc-eabivle-size.exe" in the folder "${VLE_TOOLCHAIN_DIR}/bin".

It is very appreciated for your help! 

pastedImage_3.pngpastedImage_5.png

Labels (1)
1 Solution
2,595 Views
Tangsheng_Zhou
NXP Employee
NXP Employee

Hi, Jiri Kral.

I think I fix the issue. I checked out the C/C++ Build -> Setting -> Build Artifact, and I found out that I configured the Artifact Type into E200 Library not E200 Executable. When I modified, I could build successfully.

Finally, thank you so much.

Best Regards.

Tangsheng Zhou (周塘胜)

VDS Systems&Application Engineer

Automotive Microcontrollers and Processors, China.

3F, No.10 Building, No.22 Jinyu Avenue, Liangjiang New District

Chongqing, 401122.

Mobile: +86 17388280079

Email: tangsheng.zhou@nxp.com<mailto:tangsheng.zhou@nxp.com>

发件人: jiri.kral@nxp.com <admin@community.nxp.com>

发送时间: Tuesday, September 17, 2019 11:37 PM

收件人: Tangsheng Zhou <tangsheng.zhou@nxp.com>

主题: Re: - Re: S32DS build problem about MPC5775B project

NXP Community <https://eur01.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.freescale.com%2Fresources%2Fstatics%2F1000%2F35400-NXP-Community-Email-banner-600x75.jpg&data=02%7C01%7Ctangsheng.zhou%40nxp.com%7C45b5f30e77904db099d608d73b84df73%7C686ea1d3bc2b4c6fa92cd99c5c301635%7C0%7C0%7C637043314178614380&sdata=6J6Ej0%2FODKGB1nSMHEPqPBdJRCF4LR%2FIasZMCAv%2FQVU%3D&reserved=0>

Re: S32DS build problem about MPC5775B project

reply from Jiri Kral<https://eur01.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.nxp.com%2Fpeople%2Fjiri.kral%40nxp.com%3Fet%3Dwatches.email.thread&data=02%7C01%7Ctangsheng.zhou%40nxp.com%7C45b5f30e77904db099d608d73b84df73%7C686ea1d3bc2b4c6fa92cd99c5c301635%7C0%7C0%7C637043314178624375&sdata=Or3JGltz79Z2r0s8ChHIRdZoiKcVEqbjX%2FxC1bKRqoI%3D&reserved=0> in S32 Design Studio - View the full discussion<https://eur01.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.nxp.com%2Fmessage%2F1207133%3FcommentID%3D1207133%26et%3Dwatches.email.thread%23comment-1207133&data=02%7C01%7Ctangsheng.zhou%40nxp.com%7C45b5f30e77904db099d608d73b84df73%7C686ea1d3bc2b4c6fa92cd99c5c301635%7C0%7C0%7C637043314178624375&sdata=tT1NFbEmLaICHvh2sNlXKZE7iM0gi1pDc%2BWRBU3z9Ms%3D&reserved=0>

View solution in original post

3 Replies
2,595 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

sorry for delay. What is your size settings? 

pastedImage_2.png

Jiri

0 Kudos
2,596 Views
Tangsheng_Zhou
NXP Employee
NXP Employee

Hi, Jiri Kral.

I think I fix the issue. I checked out the C/C++ Build -> Setting -> Build Artifact, and I found out that I configured the Artifact Type into E200 Library not E200 Executable. When I modified, I could build successfully.

Finally, thank you so much.

Best Regards.

Tangsheng Zhou (周塘胜)

VDS Systems&Application Engineer

Automotive Microcontrollers and Processors, China.

3F, No.10 Building, No.22 Jinyu Avenue, Liangjiang New District

Chongqing, 401122.

Mobile: +86 17388280079

Email: tangsheng.zhou@nxp.com<mailto:tangsheng.zhou@nxp.com>

发件人: jiri.kral@nxp.com <admin@community.nxp.com>

发送时间: Tuesday, September 17, 2019 11:37 PM

收件人: Tangsheng Zhou <tangsheng.zhou@nxp.com>

主题: Re: - Re: S32DS build problem about MPC5775B project

NXP Community <https://eur01.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.freescale.com%2Fresources%2Fstatics%2F1000%2F35400-NXP-Community-Email-banner-600x75.jpg&data=02%7C01%7Ctangsheng.zhou%40nxp.com%7C45b5f30e77904db099d608d73b84df73%7C686ea1d3bc2b4c6fa92cd99c5c301635%7C0%7C0%7C637043314178614380&sdata=6J6Ej0%2FODKGB1nSMHEPqPBdJRCF4LR%2FIasZMCAv%2FQVU%3D&reserved=0>

Re: S32DS build problem about MPC5775B project

reply from Jiri Kral<https://eur01.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.nxp.com%2Fpeople%2Fjiri.kral%40nxp.com%3Fet%3Dwatches.email.thread&data=02%7C01%7Ctangsheng.zhou%40nxp.com%7C45b5f30e77904db099d608d73b84df73%7C686ea1d3bc2b4c6fa92cd99c5c301635%7C0%7C0%7C637043314178624375&sdata=Or3JGltz79Z2r0s8ChHIRdZoiKcVEqbjX%2FxC1bKRqoI%3D&reserved=0> in S32 Design Studio - View the full discussion<https://eur01.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.nxp.com%2Fmessage%2F1207133%3FcommentID%3D1207133%26et%3Dwatches.email.thread%23comment-1207133&data=02%7C01%7Ctangsheng.zhou%40nxp.com%7C45b5f30e77904db099d608d73b84df73%7C686ea1d3bc2b4c6fa92cd99c5c301635%7C0%7C0%7C637043314178624375&sdata=tT1NFbEmLaICHvh2sNlXKZE7iM0gi1pDc%2BWRBU3z9Ms%3D&reserved=0>

2,593 Views
Tangsheng_Zhou
NXP Employee
NXP Employee

Hi, thank you for you reply.

The pictures named “print_sie1.png” and “print_size2.png” are the size settings about my project the same as “DEBUG” mode. And the file named “makefile” is the makefile of my project.

Best Regards.

Tangsheng Zhou (周塘胜)

VDS Systems&Application Engineer

Automotive Microcontrollers and Processors, China.

3F, No.10 Building, No.22 Jinyu Avenue, Liangjiang New District

Chongqing, 401122.

Mobile: +86 17388280079

Email: tangsheng.zhou@nxp.com<mailto:tangsheng.zhou@nxp.com>

发件人: jiri.kral@nxp.com <admin@community.nxp.com>

发送时间: Tuesday, September 17, 2019 11:37 PM

收件人: Tangsheng Zhou <tangsheng.zhou@nxp.com>

主题: Re: - Re: S32DS build problem about MPC5775B project

NXP Community <https://eur01.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.freescale.com%2Fresources%2Fstatics%2F1000%2F35400-NXP-Community-Email-banner-600x75.jpg&data=02%7C01%7Ctangsheng.zhou%40nxp.com%7C45b5f30e77904db099d608d73b84df73%7C686ea1d3bc2b4c6fa92cd99c5c301635%7C0%7C0%7C637043314178614380&sdata=6J6Ej0%2FODKGB1nSMHEPqPBdJRCF4LR%2FIasZMCAv%2FQVU%3D&reserved=0>

Re: S32DS build problem about MPC5775B project

reply from Jiri Kral<https://eur01.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.nxp.com%2Fpeople%2Fjiri.kral%40nxp.com%3Fet%3Dwatches.email.thread&data=02%7C01%7Ctangsheng.zhou%40nxp.com%7C45b5f30e77904db099d608d73b84df73%7C686ea1d3bc2b4c6fa92cd99c5c301635%7C0%7C0%7C637043314178624375&sdata=Or3JGltz79Z2r0s8ChHIRdZoiKcVEqbjX%2FxC1bKRqoI%3D&reserved=0> in S32 Design Studio - View the full discussion<https://eur01.safelinks.protection.outlook.com/?url=https%3A%2F%2Fcommunity.nxp.com%2Fmessage%2F1207133%3FcommentID%3D1207133%26et%3Dwatches.email.thread%23comment-1207133&data=02%7C01%7Ctangsheng.zhou%40nxp.com%7C45b5f30e77904db099d608d73b84df73%7C686ea1d3bc2b4c6fa92cd99c5c301635%7C0%7C0%7C637043314178624375&sdata=tT1NFbEmLaICHvh2sNlXKZE7iM0gi1pDc%2BWRBU3z9Ms%3D&reserved=0>

0 Kudos