S32DS Vision:Segmentation fault

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32DS Vision:Segmentation fault

跳至解决方案
1,928 次查看
liujinbao
Contributor II

hello:

I use the board SBC_S32V234.

The BSP version I am using is VisionSDK_S32V2_RTM_1_3_0_img_yocto.

On the official website,the file name is as follows (yellow box):

pastedImage_1.png
S32DS_Vision_v2.0 is installed on windows7 64.
After I compiled isp_sonyimx224_sci_dcu:A53_Linux, the generated executable file was sent to the development board via SSH, and the execution failed, as shown below:

1.png

0 项奖励
回复
1 解答
1,818 次查看
liujinbao
Contributor II

After replacing S32DS_Vision_v2.0 with S32DS_Vision_2018.R1, the routine can be executed normally.

1.png

thanks!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,818 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

S32DS for Vision v2.0 contains VSDK RTM v1.0.0. Some examples aren't compatible with OS image from VSDK RTM v1.3.0. Please use OS image which comes with S32DS Installation. 

Or you can use new S32DS - https://community.nxp.com/docs/DOC-342080

Jiri 

0 项奖励
回复
1,819 次查看
liujinbao
Contributor II

After replacing S32DS_Vision_v2.0 with S32DS_Vision_2018.R1, the routine can be executed normally.

1.png

thanks!

0 项奖励
回复