S32DS Licence Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32DS Licence Problem

跳至解决方案
842 次查看
greyes
Contributor II

Hello,

I am not able to reinstall S32DS due to a licence problem. (Fullfillment ID 197733417)

I cannot return the licence or remove it from my account. I do not have S32DS currently installed.

 

Also, what is the correct procedure so that this does not happen again?

Thank you!

 

greyes_0-1726750893838.png

 

标记 (2)
0 项奖励
回复
1 解答
825 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @greyes 

I think you are confused, the licenses shown are not for S32 Design Studio for the S32 platform, they are S32K3 software licenses. I cannot determine which one it is, but if you press the "Details" button it will send you to a page that provides all the details of the license.

You can find the S32DS activation code directly on the IDE page: S32 Design Studio 3.5 > S32 Design Studio for S32 Platform v.3.5 > License Keys tab. 

 

BR, VaneB

在原帖中查看解决方案

0 项奖励
回复
1 回复
826 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @greyes 

I think you are confused, the licenses shown are not for S32 Design Studio for the S32 platform, they are S32K3 software licenses. I cannot determine which one it is, but if you press the "Details" button it will send you to a page that provides all the details of the license.

You can find the S32DS activation code directly on the IDE page: S32 Design Studio 3.5 > S32 Design Studio for S32 Platform v.3.5 > License Keys tab. 

 

BR, VaneB

0 项奖励
回复