S32DS IDE是否有类似KEIL的User功能,在编译完成后可用执行一个脚本

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS IDE是否有类似KEIL的User功能,在编译完成后可用执行一个脚本

Jump to solution
991 Views
cnubsq
Contributor II

S32DS是否有如下图类似KEIL的功能:

cnubsq_0-1659511529421.png

 

0 Kudos
Reply
1 Solution
962 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can use pre-build and post-build commands in S32DS (it can be configured in Project Properties): 

jiri_kral_0-1660042875472.png

 

View solution in original post

1 Reply
963 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can use pre-build and post-build commands in S32DS (it can be configured in Project Properties): 

jiri_kral_0-1660042875472.png