S32DS For Power Architecture

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS For Power Architecture

1,498 次查看
kmh48301
Contributor IV

Hello.

I need to use S32DS For Power Architecture IDE and M(S)PC 5775E MCU

And I need to make Library File (.a file) for it with GHS Compiler.

So i have installed and imported the GHS Compiler to S32DS For Power Architecture.

 

But I can't make Library File.

kmh48301_0-1655952402917.png

I can't see the GHS Toolchain in the selection bar.

 

when i create application project, i can see it.

kmh48301_1-1655952469038.png

 

 

Can you please give me a little hand?

I've already asked to my compiler vendor.

But he told me to ask to NXP.

 

Thanks.

Best Regards.

Phillip.

0 项奖励
回复
1 回复

1,453 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @kmh48301,

First, use the wizard to create an application project, selecting GHS as the toolchain, then follow the steps in the attached document.

Best Regards,

Mike

0 项奖励
回复