S32DS EWL and NewLib

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS EWL and NewLib

4,799 次查看
nxf47968
NXP Employee
NXP Employee

Hello,

So I am new to S32DS and have a problem understanding a few parameters regarding the EWL and NewLib libraries for the project.

I have a general idea as to what the libraries are from  S32DS EWL and newlib standard clarification 

Q1. On creating a new S32R274 Project, under project properties, there following Library supports. What are all these libraries? What id the difference between ewl_c no I/O, ewl_c Debugger console and ewl_c9x? How can I know Where can I get information on all the different specs? 

pastedImage_4.png

-Su

标记 (3)
2 回复数

3,748 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

the I/O and no I/O means that with I/O you can use printf functionality via Debug probe. 

The specs option shows which gcc args set was used for library build. You can find these files in S32DS Instalation - [YOUR_INSTALL_PATH]\S32DS_Power_v2017.R1\S32DS\e200_ewl2\lib\

for newlib are .specs located here: 

[YOUR_INSTALL_PATH]\S32DS_Power_v2017.R1\Cross_Tools\powerpc-eabivle-4_9\powerpc-eabivle\newlib\lib\

Hope it helps. 

Jiri 

3,748 次查看
hanisamara
Contributor III

Hello Jiri, 

i am trying to create a c++ project under S32DS for KEA128 Controller with newLib_nano no IO. But when i build the project (empty, just main) the code size is about 47k? did i miss anything to set? i did the same with a C Project and the code size is less than 1k? 

another question: if i do not want to use any printf, strings or any library functions, can i set the library support option to none? if i do this i get many linker errors?

thanks in advance, 

Hani 

0 项奖励
回复